According to the documentation available in the MAXM86146 software package, the internal microcontroller has drivers for the only 2 accelerometers: KX122 and the LIS2DS12.
However, an alternative is…
The AFE_GPI pin of the MAXM86146 does not have an internal pull-up resistor. In this case, an external pull up resistor is needed to, as the GPIO is open-drain (active low) when used as an output.
The AFE_GPI pin of the MAXM86146 does not have an internal pull-up resistor. In this case, an external pull up resistor is needed to, as the GPIO is open-drain (active low) when used as an output as shown…
The V IH and V IL levels for the 32KIN pin should be the same as the GPIO, but since this pin is not characterized specifically during production, the voltage tolerances for this pin as well as its rising…
AGC is a subset of AEC. In AEC, the MAXM86146 controls most of the AFE's settings, while in AGC, you need to control the PD (Photodiode) current. The best fit between AGC and AEC depends on your algorithm…
Here are the details of the spacing of the PDs integrated with the MAXM86146:
The recommended spacing between Green LED and PD active edge is 2.5mm, and for RED and IR LEDs and Active Edge of the PD…
The MAXM86146 integrates both the MAX86141 and MAX32664 into a single package. Therefore, you can refer to the register documentation for those components when working with the MAXM86146.