Article Why is the message "HR/SPO2 only valid for Fs=100Sps" displayed in the MAX30102ACCEVKIT GUI?

Even though the MAX30102 datasheet says that other sampling rates can be selected for the part, the MAX30102ACCEVKIT GUI displays the message "HR/SPO2 only valid for Fs=100Sps" due to the internal algorithms written for the device to calculate heart rate (HR) and peripheral capillary oxygen saturation (SpO2).  They require a sampling rate of 100Sps. This does not reflect the capability of the device itself.  Also, customers can still log the PPG samples using the evaluation kit.




Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.