Skip navigation

News

Announcement 1 EngineerZone will be READ ONLY August 22-28. Click Show Details for more.
Announcement:EngineerZone will be READ ONLY August 22-28. Click Show Details for more.
Announcement 2 August 28th: EngineerZone will be unavailable for up to 7 hoursAnnouncement count

Top & Trending
asadali4651
Dear Fellow Engineers    i am new to the engineering community and currently working with AD9361. Through out my research so far, i have seen the Presence of DC Offset (DC Leakage from Mixer inside ad9361) on the TX side as shown below in attachment. This is the something that i would like to remove or minimize even more so that it is
3

pierrelouis
Hi, I have AD9361 FMComms5 with Xilinx ZCU102. I am using IIO Oscilloscope which worked correctly after booting with SD Card. However, I noticed I haven't the FMComms5 Advanced Plugin on IIO. How can I had this plugin on it ? Is there anything to write on the linux terminal to add it ? I need this plugin to synchronize the two AD9361 using MCS
5