Locale Icon
English
EngineerZone
EngineerZone
Motor Control Hardware Platforms
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
    Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
    • COTS SoMs & Phased Array Solutions for Rapid RF Subsystem Integration
    • LEO Satcom: Application of RF, Mixed-Signal, & Beamforming ICs
    • 3 Real World Methods to Make Your Power Supply More Intelligent
    • Revolutionizing Flow Cytometry: 20-Bit Precision Signal Chain
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quiz AQQ300 about Divisibility by 6

      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Clock Tree Design and Why “PLL Locked” Is Not Enough

    In high-performance RF systems, clocking architecture is a foundational element that directly governs signal integrity, synchronization, and overall system...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Improving Industrial Functional Safety Compliance with High Performance Supervisory CircuitsPart 5: Sequencers Eliminate Systematic Failures

    This article shifts focus from managing the quantitative metrics of functional safety toward mastering the qualitative yet equally critical challenge:...

Motor Control Hardware Platforms
Motor Control Hardware Platforms
Documents Sample C Code for EV-MCS-LVDRV-Z (FlexMC LV) platform
  • Forums
  • FAQs/ Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADIMonitor: FAQ
  • +Arduino: FAQ
  • +CM40x: FAQ
  • -Code Examples: FAQ
    • ADSP-CM40x Encoder example
    • ADSP-CM40x PWM example
    • ADSP-CM40x Software Enablement Package v2.0.0
    • ADSP-CM40x SW Enablement Package ver. 1.2.0
    • Getting Started with the EV-MCS-ISOINVEP-Z Platform
    • Sample C Code for EV-MCS-LVDRV-Z (FlexMC LV) platform
    • Sample C code for Isolated Inverter Platform (EV-MCS-ISOINV-Z)
  • +Firmware: FAQ
  • +HPPWM: FAQ
  • +Motor Control: FAQ
  • +Motors: FAQ
  • +PCB Guidelines: FAQ
  • +Platform Schematics: FAQ
  • +Raspberry Pi: FAQ
  • +Specific Products: FAQ
  • +Technical: FAQ
  • +TMCL: FAQ
  • Topic: FAQ
  • Trinamic Customs: FAQ

Sample C Code for EV-MCS-LVDRV-Z (FlexMC LV) platform

The attached zip file contains an IAR Embedded Workbench project with sample C code that can be loaded on to an ADSP-CM408 EZkit for development of a motor control application. The sample code contains an open loop Volts/Hertz algorithm that can be run in conjunction with the EV-MCS-LVDRV-Z motor control platform. The Windows Graphical User Interface (and associated user guide) found here can be used to get a motor up and running with the boards. The ADI Software Enablement (SWE) Package, to which the user guide refers, must also be downloaded and installed.


The following should be noted:

LED1 on EZkit flashing regularly - motor control algorithm is running

LED2 on EZkit is ON - PWM trip has occurred due to overcurrent. Press 'Stop' on the GUI to send a Stop Motor command. This should reset the error, and the LED should turn off.

The following Project Options also need to be set in IAR Embedded Workbench:

General Options->Target->Device=AnalogDevices ADSP-CM40z-384_2048 (will only be visible after the ADI SWE has been installed). On same tab an FPU must be selected

General Options->Library Configuration- Select Use CMSIS and DSP Library

C/C++ Compiler->Preprocessor->Additional include directories

C:\Analog Devices\ADSP-CM40x\CM403F_CM408F_EZ-KIT\inc

C:\Analog Devices\ADSP-CM40x\CM403F_CM408F_EZ-KIT\inc\sys

C:\Analog Devices\ADSP-CM40x\CM403F_CM408F_EZ-KIT\src

$PROJ_DIR$\..\MotorControl\

$PROJ_DIR$\..\System\

$PROJ_DIR$\..\Measure\

$PROJ_DIR$\..\ADIMonitorLibrary\inc\

On the same tab: Defined symbols

ARM_MATH_CM4

Linker->Library->Additional libraries

C:\Analog Devices\ADSP-CM40x\CM403F_CM408F_EZ-KIT\lib\iar\debug\libdrv40z.a

C:\Analog Devices\ADSP-CM40x\CM403F_CM408F_EZ-KIT\lib\iar\debug\libosal40z_noos.a

C:\Analog Devices\ADSP-CM40x\CM403F_CM408F_EZ-KIT\lib\iar\debug\libssl40z.a

$PROJ_DIR$\..\ADIMonitorLibrary\lib\ADI_Monitor_Library.a

Linker->List- Select Generate linker map file

Options->Debugger->Download- Select Use flash loader

Options->Debugger->J-Link/J-Trace->Setup -Select Connect during reset

Options->Debugger->J-Link/J-Trace->Connection - Select SWD

Attachments:
7485.OpenLoopSampleCode.zip
Tags: motor drive Code Examples adsp-cm40xx motor_control motor control