Locale Icon
English
EngineerZone
EngineerZone
Motor Control Hardware Platforms
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
    Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp open looop gain and LTspice (a kind proposal from Al Butvidas)

      1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits next to you and says 'wasn't that...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Understanding Voltage Domain Isolation in Field-Bus...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Dont Let Your Feedback Loop Fall FlatPart 2: Dynamic Response and Isolation Innovation!

    Introduction In isolated power supply systems, maintaining a stable output voltage under varying load conditions is essential for reliable operation. The...

Motor Control Hardware Platforms
Motor Control Hardware Platforms
Documents How can I change from CANopen firmware to TMCL firmware?
  • Forums
  • FAQs/ Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADIMonitor: FAQ
  • +Arduino: FAQ
  • +CM40x: FAQ
  • +Code Examples: FAQ
  • +Firmware: FAQ
  • +HPPWM: FAQ
  • +Motor Control: FAQ
  • +Motors: FAQ
  • +PCB Guidelines: FAQ
  • +Platform Schematics: FAQ
  • +Raspberry Pi: FAQ
  • +Specific Products: FAQ
  • +Technical: FAQ
  • -TMCL: FAQ
    • Can I load a TMCL file to a module without using the TMCL-IDE?
    • How can I change from CANopen firmware to TMCL firmware?
    • How can I change the ID of a module?
    • How can I enable autostart?
    • How do I control a module or Evaluation Kit with Matlab?
    • How do I implement a FOR loop in TMCL?
    • How do I implement Timer Interrupt in TMCL?
    • How do I send a TMCL program to the module?
    • How do I set an interrupt input change?
    • How do I use the StallGuard interrupt?
    • How do I use the X-register?
    • Is there a TMCL code library?
    • What is TMCL?
    • Where can I find the TMCL creator?
  • Topic: FAQ
  • Trinamic Customs: FAQ

How can I change from CANopen firmware to TMCL firmware?

When you have a module with CANopen firmware, the red LED flashes when CAN is not connected. With CANopen firmware, it is not possible to control the motor using the TMCL-IDE or TMCL commands.

However, you can turn the CANopen module into a TMCL module using a firmware update. Get the TMCL firmware file from the product page of the module on our website and then use the firmware update function of the TMCL-IDE to perform the firmware update. 

There are two options to do so:

  1. If the module offers USB, just connect the module via USB. Do not connect the power supply (otherwise USB would not work with CANopen firmware).
  2. When updating the firmware via CAN, you first have to put the module into bootloader mode. To do so, click on the connected CAN-adapter in the TMCL-IDE and click on "Send boot command" in the CANopen-tab. After restarting the IDE you are able to perform the firmware update with the update function.