Locale Icon
English
EngineerZone
EngineerZone
Motor Control Hardware Platforms
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
    Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
    • LEO Satcom: Application of RF, Mixed-Signal, & Beamforming ICs
    • 3 Real World Methods to Make Your Power Supply More Intelligent
    • Revolutionizing Flow Cytometry: 20-Bit Precision Signal Chain
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quiz AQQ300 about Divisibility by 6

      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Clock Tree Design and Why “PLL Locked” Is Not Enough

    In high-performance RF systems, clocking architecture is a foundational element that directly governs signal integrity, synchronization, and overall system...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    The Right Switch-Mode Power Supply Control Scheme

    This article compares three switch-mode power supply control schemescurrent-mode control, voltage-mode control, and hysteretic-mode control to guide engineers...

Motor Control Hardware Platforms
Motor Control Hardware Platforms
Documents How do I use the X-register?
  • Forums
  • FAQs/ Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADIMonitor: FAQ
  • +Arduino: FAQ
  • +CM40x: FAQ
  • +Code Examples: FAQ
  • +Firmware: FAQ
  • +HPPWM: FAQ
  • +Motor Control: FAQ
  • +Motors: FAQ
  • +PCB Guidelines: FAQ
  • +Platform Schematics: FAQ
  • +Raspberry Pi: FAQ
  • +Specific Products: FAQ
  • +Technical: FAQ
  • -TMCL: FAQ
    • Can I load a TMCL file to a module without using the TMCL-IDE?
    • How can I change from CANopen firmware to TMCL firmware?
    • How can I change the ID of a module?
    • How can I enable autostart?
    • How do I control a module or Evaluation Kit with Matlab?
    • How do I implement a FOR loop in TMCL?
    • How do I implement Timer Interrupt in TMCL?
    • How do I send a TMCL program to the module?
    • How do I set an interrupt input change?
    • How do I use the StallGuard interrupt?
    • How do I use the X-register?
    • Is there a TMCL code library?
    • What is TMCL?
    • Where can I find the TMCL creator?
  • Topic: FAQ
  • Trinamic Customs: FAQ

How do I use the X-register?

The following program demonstrates use of the X-register. Motor 0 is performing 10 rotations with velocity 1000, after which the program will be stopped.

Before use: Restore Factory Defaults.

// *** Values that have to be adapted *** // 
vmax = 2000 //max. speed (0 ... 2047)
amax = 1000 //max. acceleration (0 ... 2047)
cmax = 100 //max. current (0 ... 255)

// *** Interrupt initialization *** //
SAP 4, 0, vmax //set max. positioning speed
SAP 5, 0, amax //set max. acceleration
SAP 6, 0, cmax //set max. current

CALC LOAD, 1 //load 1 to accu
CALCX LOAD //load accu to X-register
CALC LOAD, 0 //load 0 to accu

// *** Main Loop *** //
loop:
MVP REL, 0, 51200 //perform 1 rotation: 51200 = 200 * 256
WAIT POS, 0, 0 //wait until postion reached
WAIT TICKS, 0, 100 //wait 1 second. 100 * 10ms
CALCX ADD //add X-register to accu
COMP 10 //compare accu with 10
JC LT, loop //if greater or equal 10 end program
STOP //end of program