Locale Icon
English
EngineerZone
EngineerZone
Motor Control Hardware Platforms
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
    • LiDAR Solutions
    • Motor Control Hardware Platforms
    • Speech Processing Solutions
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
    Accelerate RF Subsystem Integration with COTS SoMs and Phased Array Solutions. As building a subsystem from early prototype to full deployment is never...
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
      KCC's Quizzes AQQ301 - Counting Bicycles and Tricycles

      1. Quote of the month: " People who didn't need people needed people around to know that they were the kind of people who didn't need people" - Terry Pratchett...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 2: Achieving Phase Repeatability

    This article discusses a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a...

Motor Control Hardware Platforms
Motor Control Hardware Platforms
Documents How do I implement Timer Interrupt in TMCL?
  • Forums
  • FAQs/ Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADIMonitor: FAQ
  • +Arduino: FAQ
  • +CM40x: FAQ
  • +Code Examples: FAQ
  • +Firmware: FAQ
  • +HPPWM: FAQ
  • +Motor Control: FAQ
  • +Motors: FAQ
  • +PCB Guidelines: FAQ
  • +Platform Schematics: FAQ
  • +Raspberry Pi: FAQ
  • +Specific Products: FAQ
  • +Technical: FAQ
  • -TMCL: FAQ
    • Can I load a TMCL file to a module without using the TMCL-IDE?
    • How can I change from CANopen firmware to TMCL firmware?
    • How can I change the ID of a module?
    • How can I enable autostart?
    • How do I control a module or Evaluation Kit with Matlab?
    • How do I implement a FOR loop in TMCL?
    • How do I implement Timer Interrupt in TMCL?
    • How do I send a TMCL program to the module?
    • How do I set an interrupt input change?
    • How do I use the StallGuard interrupt?
    • How do I use the X-register?
    • Is there a TMCL code library?
    • What is TMCL?
    • Where can I find the TMCL creator?
  • Topic: FAQ
  • Trinamic Customs: FAQ

How do I implement Timer Interrupt in TMCL?

This program below demonstrates how to use the timer interrupt.

To use this program, connect LEDs to OUT_0 and OUT_1. The LED at port OUT_1 is toggling at 2 Hz using the WAIT command. Connect a LED to port OUT_0. This LED connected to OUT_0 will be toggling at 1 Hz using the timer interrupt.

Before use: Restore Factory Defaults.

        // *** Interrupt initialization *** // 
VECT 0, Timer0Irq //defines the interrupt vector for the timer 0 interrupt
SGP 0, 3, 1000 //configure the timer interrupt: set its period to 1000ms
EI 0 //enable timer interrupt
EI 255 //globally switch on interrupt processing

// *** Main Loop *** //
loop:
SIO 1, 2, 1 //switch OUT_1 high
WAIT TICKS, 0, 50 //wait 0.5 seconds. 50 * 10ms
SIO 1, 2, 0 //switch OUT_1 low
WAIT TICKS, 0, 50 //wait 0.5 seconds. 50 * 10ms
JA loop //jump to loop
// *** Interrupt routine *** //
Timer0Irq:
GIO 0, 2 //check if OUT_0 is high
JC NZ, Out0Off //jump to Out0off if high
SIO 0, 2, 1 //switch OUT_0 high
RETI //end of interrupt
Out0Off:
SIO 0, 2, 0 //switch OUT_0 low
RETI //end of interrupt