Locale Icon
English
EngineerZone
EngineerZone
Motor Control Hardware Platforms
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
    • LiDAR Solutions
    • Motor Control Hardware Platforms
    • Speech Processing Solutions
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
    Accelerate RF Subsystem Integration with COTS SoMs and Phased Array Solutions. As building a subsystem from early prototype to full deployment is never...
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
      KCC's Quizzes AQQ301 - Counting Bicycles and Tricycles

      1. Quote of the month: " People who didn't need people needed people around to know that they were the kind of people who didn't need people" - Terry Pratchett...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 2: Achieving Phase Repeatability

    This article discusses a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a...

Motor Control Hardware Platforms
Motor Control Hardware Platforms
Documents How do I send a TMCL program to the module?
  • Forums
  • FAQs/ Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADIMonitor: FAQ
  • +Arduino: FAQ
  • +CM40x: FAQ
  • +Code Examples: FAQ
  • +Firmware: FAQ
  • +HPPWM: FAQ
  • +Motor Control: FAQ
  • +Motors: FAQ
  • +PCB Guidelines: FAQ
  • +Platform Schematics: FAQ
  • +Raspberry Pi: FAQ
  • +Specific Products: FAQ
  • +Technical: FAQ
  • -TMCL: FAQ
    • Can I load a TMCL file to a module without using the TMCL-IDE?
    • How can I change from CANopen firmware to TMCL firmware?
    • How can I change the ID of a module?
    • How can I enable autostart?
    • How do I control a module or Evaluation Kit with Matlab?
    • How do I implement a FOR loop in TMCL?
    • How do I implement Timer Interrupt in TMCL?
    • How do I send a TMCL program to the module?
    • How do I set an interrupt input change?
    • How do I use the StallGuard interrupt?
    • How do I use the X-register?
    • Is there a TMCL code library?
    • What is TMCL?
    • Where can I find the TMCL creator?
  • Topic: FAQ
  • Trinamic Customs: FAQ

How do I send a TMCL program to the module?

First of all, you will have to assemble your program using our TMCL-IDE and save the result as a binary file. To do that, choose "Options" in the menu named "TMCL" of the TMCL Creator. There, enable the option "Write output to binary file". Now, assemble your program, and the result will be saved in a binary file. This file will have the same name as your TMCL file, but with the extension ".BIN".

This binary file contains all the TMCL commands of your program in binary format. Each command saved is eight bytes: It is the command without the module address.

Once you have this file with the commands needed for your application, proceed as following:

  1. Send command 132 (enter download mode), with type, motor/bank and value set to 0.
  2. Open the binary file.
  3. Read 8 bytes from the file.
  4. Add the module address of your module (in most cases 1) to the 8 bytes (so that the check sum is correct).
  5. Send the module address (in most cases 1) and the 8 bytes to the module.
  6. You will get a reply (9 bytes) with the status set to 101 (which means that the command has been stored in the EEPROM).
  7. If you are not at the end of the file, go to step (3).
  8. Send a command opcode 0 to the module (with module address 1 this would be 0x01 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x01). This is just an end marker for the disassembler in the TMCL-IDE.
  9. Send command 133 (exit download mode), with type, motor/bank and value set to 0.

That's all. You can check if it works by using the "Disassemble" function of the TMCL-IDE.