Locale Icon
English
EngineerZone
EngineerZone
Motor Control Hardware Platforms
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
    Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp open looop gain and LTspice (a kind proposal from Al Butvidas)

      1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits next to you and says 'wasn't that...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Understanding Voltage Domain Isolation in Field-Bus...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

Motor Control Hardware Platforms
Motor Control Hardware Platforms
Documents How do I set an interrupt input change?
  • Forums
  • FAQs/ Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADIMonitor: FAQ
  • +Arduino: FAQ
  • +CM40x: FAQ
  • +Code Examples: FAQ
  • +Firmware: FAQ
  • +HPPWM: FAQ
  • +Motor Control: FAQ
  • +Motors: FAQ
  • +PCB Guidelines: FAQ
  • +Platform Schematics: FAQ
  • +Raspberry Pi: FAQ
  • +Specific Products: FAQ
  • +Technical: FAQ
  • -TMCL: FAQ
    • Can I load a TMCL file to a module without using the TMCL-IDE?
    • How can I change from CANopen firmware to TMCL firmware?
    • How can I change the ID of a module?
    • How can I enable autostart?
    • How do I control a module or Evaluation Kit with Matlab?
    • How do I implement a FOR loop in TMCL?
    • How do I implement Timer Interrupt in TMCL?
    • How do I send a TMCL program to the module?
    • How do I set an interrupt input change?
    • How do I use the StallGuard interrupt?
    • How do I use the X-register?
    • Is there a TMCL code library?
    • What is TMCL?
    • Where can I find the TMCL creator?
  • Topic: FAQ
  • Trinamic Customs: FAQ

How do I set an interrupt input change?

The short program below demonstrates how to set the interrupt on an input change in TMCL. The behavior of this program is the same as EX0008. Depending on the status of Port IN_0, motor 0 turns right (IN_0 = 0) or left (IN_0 = 1).

Before use: Restore Factory Defaults.

// *** Values that have to be adapted *** // 
amax = 1000 //max. acceleration (0 ... 2047)
vmax = 2000 //max. speed (0 ... 2047)
cmax = 100 //max. current (0 ... 255)

// *** Initialization / Set up axis parameter *** //
SAP 5, 0, amax //set max. acceleration
SAP 6, 0, cmax //set max. current

// *** Interrupt initialization *** //
VECT 39, changeRotation //define the interrupt vector for input change 0 interrupt (IN_0)
SGP 39, 3, 3 //configure interrupt to trigger on both edge of input 0 (0=off,1=low-high,2=high-low,3=both)
EI 39 //enable input change 0 interrupt (IN_0)
EI 255 //globally switch on interrupt processing

// *** Main Loop *** //
loop: //infinite loop
JA loop //jump to loop

changeRotation:
GIO 0, 0 //read IN_0
COMP 0 //compare with 0
JC EQ, turnRight //if equal jump to turn right R
ROL 0, vmax //if not equal turn left at vmax
RETI //end of interrupt
turnRight:
ROR 0, vmax //turn right at vmax
RETI //end of interrupt