Locale Icon
English
EngineerZone
EngineerZone
Motor Control Hardware Platforms
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
    Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
    • COTS SoMs & Phased Array Solutions for Rapid RF Subsystem Integration
    • LEO Satcom: Application of RF, Mixed-Signal, & Beamforming ICs
    • 3 Real World Methods to Make Your Power Supply More Intelligent
    • Revolutionizing Flow Cytometry: 20-Bit Precision Signal Chain
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quiz AQQ300 about Divisibility by 6

      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Clock Tree Design and Why “PLL Locked” Is Not Enough

    In high-performance RF systems, clocking architecture is a foundational element that directly governs signal integrity, synchronization, and overall system...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Improving Industrial Functional Safety Compliance with High Performance Supervisory CircuitsPart 5: Sequencers Eliminate Systematic Failures

    This article shifts focus from managing the quantitative metrics of functional safety toward mastering the qualitative yet equally critical challenge:...

Motor Control Hardware Platforms
Motor Control Hardware Platforms
Documents How do I control a module or Evaluation Kit with Matlab?
  • Forums
  • FAQs/ Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADIMonitor: FAQ
  • +Arduino: FAQ
  • +CM40x: FAQ
  • +Code Examples: FAQ
  • +Firmware: FAQ
  • +HPPWM: FAQ
  • +Motor Control: FAQ
  • +Motors: FAQ
  • +PCB Guidelines: FAQ
  • +Platform Schematics: FAQ
  • +Raspberry Pi: FAQ
  • +Specific Products: FAQ
  • +Technical: FAQ
  • -TMCL: FAQ
    • Can I load a TMCL file to a module without using the TMCL-IDE?
    • How can I change from CANopen firmware to TMCL firmware?
    • How can I change the ID of a module?
    • How can I enable autostart?
    • How do I control a module or Evaluation Kit with Matlab?
    • How do I implement a FOR loop in TMCL?
    • How do I implement Timer Interrupt in TMCL?
    • How do I send a TMCL program to the module?
    • How do I set an interrupt input change?
    • How do I use the StallGuard interrupt?
    • How do I use the X-register?
    • Is there a TMCL code library?
    • What is TMCL?
    • Where can I find the TMCL creator?
  • Topic: FAQ
  • Trinamic Customs: FAQ

How do I control a module or Evaluation Kit with Matlab?

if you're looking to control a module or evaluation kit from ADI Trinamic using Mathlab, please use the short Matlab script below.

% function to move motor to positon 

% ROR Command
function move(nin)
n = int32(nin);

% generate command
% byte1 - adress
byte(1:4) = uint8([1,4,1,0]);
byte(5)= uint8(bitand(bitshift(n,-24),255) );
byte(6)= uint8(bitand(bitshift(n,-16),255) );
byte(7)= uint8(bitand(bitshift(n,-8),255) );
byte(8)= uint8(bitand(n,255) );
byte(9)=uint8(bitand(sum(byte(1:8)),255) ),

% open com port for data transfer
fid = serial('COM12','BaudRate',9600, 'DataBits', 8, 'Parity', 'none','StopBits', 1, 'FlowControl', 'none');
fopen (fid);

%send command
fwrite(fid,byte);
pause(1);

%get answer
answer = fread(fid, 9, 'uint8')

% close com port connection
fclose(fid);

% when you enter the function " move_right(1, 0.005,0.01)" in your
% window command, the motor can move.