Locale Icon
English
EngineerZone
EngineerZone
Motor Control Hardware Platforms
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
    Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp open looop gain and LTspice (a kind proposal from Al Butvidas)

      1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits next to you and says 'wasn't that...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Understanding Voltage Domain Isolation in Field-Bus...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

Motor Control Hardware Platforms
Motor Control Hardware Platforms
Documents How do I use the StallGuard interrupt?
  • Forums
  • FAQs/ Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADIMonitor: FAQ
  • +Arduino: FAQ
  • +CM40x: FAQ
  • +Code Examples: FAQ
  • +Firmware: FAQ
  • +HPPWM: FAQ
  • +Motor Control: FAQ
  • +Motors: FAQ
  • +PCB Guidelines: FAQ
  • +Platform Schematics: FAQ
  • +Raspberry Pi: FAQ
  • +Specific Products: FAQ
  • +Technical: FAQ
  • -TMCL: FAQ
    • Can I load a TMCL file to a module without using the TMCL-IDE?
    • How can I change from CANopen firmware to TMCL firmware?
    • How can I change the ID of a module?
    • How can I enable autostart?
    • How do I control a module or Evaluation Kit with Matlab?
    • How do I implement a FOR loop in TMCL?
    • How do I implement Timer Interrupt in TMCL?
    • How do I send a TMCL program to the module?
    • How do I set an interrupt input change?
    • How do I use the StallGuard interrupt?
    • How do I use the X-register?
    • Is there a TMCL code library?
    • What is TMCL?
    • Where can I find the TMCL creator?
  • Topic: FAQ
  • Trinamic Customs: FAQ

How do I use the StallGuard interrupt?

TMCL is the simple way to implement your motion control application. With this series of simple coding examples, we want to provide you an easy start.

This program demonstrates the stall detection with stallGuard2Tm. Motor 0 will run until it is stalled, then MCL program flow will be interrupted and the interrupt handling routine (here: returnToZero) will be called. After the detection of a stall, the motor will run to position zero. For more details concerning stallGuard2Tm look at Application Note AN002_stallGuard2.pdf –  http://www.trinamic.com/design-center/application-notes. 

Before use: Restore Factory Defaults

// *** Values that have to be adapted *** // 
stallGuardValue = 2 //-64 = highest sensitivity ... 63 = lowest sensitivity
vmax = 2000 //max. speed (0 ... 2047)
amax = 1000 //max. acceleration (0 ... 2047)
cmax = 100 //max. current (0 ... 255)

// *** Initialization / Set up axis parameter *** //
SAP 1, 0, 0 //reset actual position to 0
SAP 4, 0, vmax //set max. positioning speed
SAP 5, 0, amax //set max. acceleration
SAP 6, 0, cmax //set max. current

// *** stallGuardTm initialization *** //
SAP 173, 0, 1 //set stallGuardTm filter disable
SAP 174, 0, stallGuardValue //stallGuardTm threshold
SAP 181, 0, 1900 //min. speed for motor to be stopped by stallGuardTm

// *** Interrupt initialization *** //
VECT 15, returnToZero //defines the interrupt vector for the stallGuardTm interrupt
EI 15 //enable stall interrupt
EI 255 //globally switch on interrupt processing

// *** Main Loop *** //
loop:
GAP 3, 0 //get current speed
JC NZ, loop //jump to loop if speed not zero
ROL 0, vmax //turn motor left at vmax
JA loop //jump to loop

// *** Interrupt routine *** //
returnToZero:
MVP ABS, 0, 0 //turn motor 0 to postion zero
WAIT POS, 0, 0 //wait until position zero reached
WAIT TICKS, 0, 500 //wait 5 seconds. 500 * 10ms
RETI //end of interrupt
  • Share
  • History
  • More
  • Cancel
 
Related Content
  • $core_v2_language.Truncate($item.HtmlName('Web'), 200, "...")
    $author.DisplayName
    $core_v2_language.Truncate($item.HtmlDescription('Web'), 200, "...")
  • TMCL: Using the stallGuard Interrupt
    TMCL: Using the stallGuard Interrupt
    EZ Blogs - TMCL is the simple way to implement your motion control application. With this series of simple coding examples we want to provide you an easy start. This program demonstrates the stall detection with...
  • Inquiry on how to code TMCL Language for coordinate setting(TMCM-6214)
    jpaulhwang
    Hi all, I want to set the coordinates using the TMCM-6214 and TMCL Language. first of all, I want to make a coordinates shown as below. I using the 2 motor(x axis-1ea, y axis-1ea) and I want the...
 
Related Content
  • $core_v2_language.Truncate($item.HtmlName('Web'), 200, "...")
    $author.DisplayName
    $core_v2_language.Truncate($item.HtmlDescription('Web'), 200, "...")
  • TMCL: Using the stallGuard Interrupt
    TMCL: Using the stallGuard Interrupt
    EZ Blogs - TMCL is the simple way to implement your motion control application. With this series of simple coding examples we want to provide you an easy start. This program demonstrates the stall detection with...
  • Inquiry on how to code TMCL Language for coordinate setting(TMCM-6214)
    jpaulhwang
    Hi all, I want to set the coordinates using the TMCM-6214 and TMCL Language. first of all, I want to make a coordinates shown as below. I using the 2 motor(x axis-1ea, y axis-1ea) and I want the...