Locale Icon
English
EngineerZone
EngineerZone
Motor Control Hardware Platforms
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
    Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp open looop gain and LTspice (a kind proposal from Al Butvidas)

      1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits next to you and says 'wasn't that...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Understanding Voltage Domain Isolation in Field-Bus...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

Motor Control Hardware Platforms
Motor Control Hardware Platforms
Documents Can I load a TMCL file to a module without using the TMCL-IDE?
  • Forums
  • FAQs/ Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADIMonitor: FAQ
  • +Arduino: FAQ
  • +CM40x: FAQ
  • +Code Examples: FAQ
  • +Firmware: FAQ
  • +HPPWM: FAQ
  • +Motor Control: FAQ
  • +Motors: FAQ
  • +PCB Guidelines: FAQ
  • +Platform Schematics: FAQ
  • +Raspberry Pi: FAQ
  • +Specific Products: FAQ
  • +Technical: FAQ
  • -TMCL: FAQ
    • Can I load a TMCL file to a module without using the TMCL-IDE?
    • How can I change from CANopen firmware to TMCL firmware?
    • How can I change the ID of a module?
    • How can I enable autostart?
    • How do I control a module or Evaluation Kit with Matlab?
    • How do I implement a FOR loop in TMCL?
    • How do I implement Timer Interrupt in TMCL?
    • How do I send a TMCL program to the module?
    • How do I set an interrupt input change?
    • How do I use the StallGuard interrupt?
    • How do I use the X-register?
    • Is there a TMCL code library?
    • What is TMCL?
    • Where can I find the TMCL creator?
  • Topic: FAQ
  • Trinamic Customs: FAQ

Can I load a TMCL file to a module without using the TMCL-IDE?

It is possible to load a TMCL file onto a Trinamic module.

First of all, you will have to assemble your program using the TMCL-IDE and save the result as a binary file. To do that, choose "Options" in the menu "TMCL" of the TMCL Creator. There, switch on the option "Write output to binary file". Now, assemble your program, and the result will be saved in a binary file. The file will have the same name as your TMCL file, but with the extension ".BIN". This file contains all the TMCL commands of your program in binary format. Each command is saved as eight bytes: it is the command without the module address.

Now there two options:

Option 1:

In your application, do the following things:

  1. Send command 132 (enter download mode), with type, motor/bank and value set to 0.
  2. Open the binary file.
  3. Read eight bytes from the file.
  4. Add the module address of your module (in most cases 1) to the eighth byte (so that the check sum is correct).
  5. Send the module address (in most cases 1) and the eight bytes to the module.
  6. You will get a reply with (9 bytes) with the status set to 101 (which means that command has been stored in the EEPROM).
  7. If you are not at the end of the file then go to step (3).
  8. Send a command opcode 0 to the module (with module address 1 this would be 0x01 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x01). This is just an end marker for the disassembler in the TMCL-IDE.
  9. Send command 133 (exit download mode), with type, motor/bank and value set to 0.

This is all. You can check if it works by using the Disassemble function of the TMCL-IDE.

If you have jump commands with labels you can additionally activate the "Generate a symbol file" option within the TMCL Options menu. In addition after assembling the program a .sym file will be generated that lists the labels with addresses you can use for your own program to jump to the corresponding label.

Or if you just would like to send a few commands, without jump commands (so that you do not need the assembler), then you can just send command 132, then send your commands, and then send command 133. After that, send command 129 to start the program.

 

Option 2:

We also have a small program that only downloads such a file (TMCLDownload.exe attached). With this program you can either download such a binary file manually, or the program can also be called with appropriate command line options on another program (which will simplify the process). Please note, it only supports the download via RS232, RS485 or USB.

 

Download the Program

  • Share
  • History
  • More
  • Cancel
 
Related Content
  • $core_v2_language.Truncate($item.HtmlName('Web'), 200, "...")
    $author.DisplayName
    $core_v2_language.Truncate($item.HtmlDescription('Web'), 200, "...")
  • How do I send a TMCL program to the module?
    stephenv
    First of all, you will have to assemble your program using our TMCL-IDE and save the result as a binary file. To do that, choose "Options" in the menu named "TMCL" of the TMCL Creator. There, enable the...
  • $core_v2_language.Truncate($item.HtmlName('Web'), 200, "...")
    $author.DisplayName
    $core_v2_language.Truncate($item.HtmlDescription('Web'), 200, "...")
 
Related Content
  • $core_v2_language.Truncate($item.HtmlName('Web'), 200, "...")
    $author.DisplayName
    $core_v2_language.Truncate($item.HtmlDescription('Web'), 200, "...")
  • How do I send a TMCL program to the module?
    stephenv
    First of all, you will have to assemble your program using our TMCL-IDE and save the result as a binary file. To do that, choose "Options" in the menu named "TMCL" of the TMCL Creator. There, enable the...
  • $core_v2_language.Truncate($item.HtmlName('Web'), 200, "...")
    $author.DisplayName
    $core_v2_language.Truncate($item.HtmlDescription('Web'), 200, "...")