Locale Icon
English
EngineerZone
EngineerZone
Motor Control Hardware Platforms
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
    Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp open looop gain and LTspice (a kind proposal from Al Butvidas)

      1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits next to you and says 'wasn't that...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Understanding Voltage Domain Isolation in Field-Bus...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

Motor Control Hardware Platforms
Motor Control Hardware Platforms
Documents USB-2-RTMI - Can't connect to the TMC4671 via RTMI / Failed to load LibFT4222.dll?
  • Forums
  • FAQs/ Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADIMonitor: FAQ
  • +Arduino: FAQ
  • +CM40x: FAQ
  • +Code Examples: FAQ
  • +Firmware: FAQ
  • +HPPWM: FAQ
  • +Motor Control: FAQ
  • +Motors: FAQ
  • +PCB Guidelines: FAQ
  • +Platform Schematics: FAQ
  • +Raspberry Pi: FAQ
  • -Specific Products: FAQ
    • Landungsbruecke - Why does the Landungsbruecke show up as “unknown” in the TMCL-IDE?
    • PyTrinamic:How to set global parameter on a Trinamic module using PyTrinamic
    • TMC2130 & TMC5130 - Can I reduce the standby power draw?
    • TMC4361(A) - How can I detect the current state of the HOME reference pin?
    • TMC4361A - How can I use STOPL (respectively STOPR) as home reference?
    • TMC4361A - How do I read out registers from the TMC21x0 through cover datagrams?
    • TMC4361A-EVAL - Can I combine this with another motion controller evaluation board?
    • TMC4361A-EVAL - How should I wire the encoder?
    • TMC4361A-EVAL - Why does the TMCL-IDE not recognize other motor drivers (e.g. TMC2160-EVAL) used with this eval board?
    • TMC4671 - How to enable space vector PWM?
    • TMC4671 - Is it normal to have a current spike if PWM is enabled?
    • TMC4671 - When using the TMC4671 with the TMC6200, why is the current ADC phase not in phase with the voltage output?
    • TMC4671 - Why does the autotuning with the TMC4671 not seem to work?
    • TMC4671 - Why don’t I get a valid reading from the analog encoder AENC pins?
    • TMC4671 - Why is the motor not reaching the specified target speed?
    • TMC4671 - Why is the motor not turning?
    • TMC4671+TMC6100-BOB - Why is the motor not running in open loop using the wizard?
    • USB-2-RTMI - Can't connect to the TMC4671 via RTMI / Failed to load LibFT4222.dll?
    • USB-2-RTMI - Why does the driver not work after a Windows update?
    • USB-2-RTMI - Why does the TMCL-IDE not see the device?
  • +Technical: FAQ
  • +TMCL: FAQ
  • Topic: FAQ
  • Trinamic Customs: FAQ

USB-2-RTMI - Can't connect to the TMC4671 via RTMI / Failed to load LibFT4222.dll?

If you receive the popup that the system does not support SSL/TLS, with the log showing ‘Failed to load LibFT4222.dll’, it could be that a recent Windows update is causing this error related to MSVCP100.dll and MSVCR100.dll.

To look into the error, please execute the following and check on the LibFT422.dll: GitHub - lucasg/Dependencies: A rewrite of the old legacy software "depends.exe" in C# for Windows devs to troubleshoot dll load dependencies issues.

The depencency program will highlight the issue. If the issue is indeed related to MSVCP100.dll and MSVCR100.dll, you can resolve this by installing the following: https://www.microsoft.com/en-gb/download/details.aspx?id=26999