Locale Icon
English
EngineerZone
EngineerZone
Motor Control Hardware Platforms
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
    Power Integrity for High Performance Measurement Systems

    Increasing data rates driven by AI workloads and the evolution from 5G to emerging 6G standards are placing new demands on electronic test and measurement...
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
      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read the Blog:  Simplified I/O: One Chip, Flexible Voltage Output, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Simplified I/O: One Chip, Flexible Voltage Outpu...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Using the Industrial I/O Framework for Easy Prototyping of Software Defined Radio (SDR) Transceivers
    Using the Industrial I/O Framework for Easy Prototyping of Software Defined Radio (SDR) Transceivers

    Introduction to Industrial I/O, libIIO, and Python software tools

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Evaluating Power Supplies with Different Compensation Settings

    Evaluating Power Supplies with Different Compensation Settings

Motor Control Hardware Platforms
Motor Control Hardware Platforms
Documents TMC4671 - When using the TMC4671 with the TMC6200, why is the current ADC phase not in phase with the voltage output?
  • Forums
  • FAQs/ Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADIMonitor: FAQ
  • +Arduino: FAQ
  • +CM40x: FAQ
  • +Code Examples: FAQ
  • +Firmware: FAQ
  • +HPPWM: FAQ
  • +Motor Control: FAQ
  • +Motors: FAQ
  • +PCB Guidelines: FAQ
  • +Platform Schematics: FAQ
  • +Raspberry Pi: FAQ
  • -Specific Products: FAQ
    • Landungsbruecke - Why does the Landungsbruecke show up as “unknown” in the TMCL-IDE?
    • PyTrinamic:How to set global parameter on a Trinamic module using PyTrinamic
    • TMC2130 & TMC5130 - Can I reduce the standby power draw?
    • TMC4361(A) - How can I detect the current state of the HOME reference pin?
    • TMC4361A - How can I use STOPL (respectively STOPR) as home reference?
    • TMC4361A - How do I read out registers from the TMC21x0 through cover datagrams?
    • TMC4361A-EVAL - Can I combine this with another motion controller evaluation board?
    • TMC4361A-EVAL - How should I wire the encoder?
    • TMC4361A-EVAL - Why does the TMCL-IDE not recognize other motor drivers (e.g. TMC2160-EVAL) used with this eval board?
    • TMC4671 - How to enable space vector PWM?
    • TMC4671 - Is it normal to have a current spike if PWM is enabled?
    • TMC4671 - When using the TMC4671 with the TMC6200, why is the current ADC phase not in phase with the voltage output?
    • TMC4671 - Why does the autotuning with the TMC4671 not seem to work?
    • TMC4671 - Why don’t I get a valid reading from the analog encoder AENC pins?
    • TMC4671 - Why is the motor not reaching the specified target speed?
    • TMC4671 - Why is the motor not turning?
    • TMC4671+TMC6100-BOB - Why is the motor not running in open loop using the wizard?
    • USB-2-RTMI - Can't connect to the TMC4671 via RTMI / Failed to load LibFT4222.dll?
    • USB-2-RTMI - Why does the driver not work after a Windows update?
    • USB-2-RTMI - Why does the TMCL-IDE not see the device?
  • +Technical: FAQ
  • +TMCL: FAQ
  • Topic: FAQ
  • Trinamic Customs: FAQ

TMC4671 - When using the TMC4671 with the TMC6200, why is the current ADC phase not in phase with the voltage output?

It is important to note the TMC6200 inverts the input signal, which needs to be taken into account by the TMC4671. As such, please set TMC4671 register ADC_I0_SCALE (0x09)/ADC_I1_SCALE(0x08) to negative -256.

  • Share
  • History
  • More
  • Cancel
 
Related Content
  • TMC4671
    TMC4671
    $core_v2_language.Truncate($item.HtmlDescription('Web'), 200, "...")
  • $core_v2_language.Truncate($item.HtmlName('Web'), 200, "...")
    $author.DisplayName
    $core_v2_language.Truncate($item.HtmlDescription('Web'), 200, "...")
  • RE: TMC4671+TMC6200 FOC矢量控制 异常跑飞情况
    koko1230
    初始化的时候需要防止有震动. 结合霍尔的初始化代码是有的. 您可以在我司的git上面查找. tmc/ic/TMC4671/TMC4671.c 里面的doEncoderInitializationMode2 应该就是结合了霍尔的初始化方法. 仅供您参考.
 
Related Content
  • TMC4671
    TMC4671
    $core_v2_language.Truncate($item.HtmlDescription('Web'), 200, "...")
  • $core_v2_language.Truncate($item.HtmlName('Web'), 200, "...")
    $author.DisplayName
    $core_v2_language.Truncate($item.HtmlDescription('Web'), 200, "...")
  • RE: TMC4671+TMC6200 FOC矢量控制 异常跑飞情况
    koko1230
    初始化的时候需要防止有震动. 结合霍尔的初始化代码是有的. 您可以在我司的git上面查找. tmc/ic/TMC4671/TMC4671.c 里面的doEncoderInitializationMode2 应该就是结合了霍尔的初始化方法. 仅供您参考.