Locale Icon
English
EngineerZone
EngineerZone
Motor Control Hardware Platforms
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
    Power Integrity for High Performance Measurement Systems

    Increasing data rates driven by AI workloads and the evolution from 5G to emerging 6G standards are placing new demands on electronic test and measurement...
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
      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read the Blog:  Simplified I/O: One Chip, Flexible Voltage Output, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Simplified I/O: One Chip, Flexible Voltage Outpu...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

Motor Control Hardware Platforms
Motor Control Hardware Platforms
Documents TMC4671 - Why is the motor not turning?
  • Forums
  • FAQs/ Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADIMonitor: FAQ
  • +Arduino: FAQ
  • +CM40x: FAQ
  • +Code Examples: FAQ
  • +Firmware: FAQ
  • +HPPWM: FAQ
  • +Motor Control: FAQ
  • +Motors: FAQ
  • +PCB Guidelines: FAQ
  • +Platform Schematics: FAQ
  • +Raspberry Pi: FAQ
  • -Specific Products: FAQ
    • Landungsbruecke - Why does the Landungsbruecke show up as “unknown” in the TMCL-IDE?
    • PyTrinamic:How to set global parameter on a Trinamic module using PyTrinamic
    • TMC2130 & TMC5130 - Can I reduce the standby power draw?
    • TMC4361(A) - How can I detect the current state of the HOME reference pin?
    • TMC4361A - How can I use STOPL (respectively STOPR) as home reference?
    • TMC4361A - How do I read out registers from the TMC21x0 through cover datagrams?
    • TMC4361A-EVAL - Can I combine this with another motion controller evaluation board?
    • TMC4361A-EVAL - How should I wire the encoder?
    • TMC4361A-EVAL - Why does the TMCL-IDE not recognize other motor drivers (e.g. TMC2160-EVAL) used with this eval board?
    • TMC4671 - How to enable space vector PWM?
    • TMC4671 - Is it normal to have a current spike if PWM is enabled?
    • TMC4671 - When using the TMC4671 with the TMC6200, why is the current ADC phase not in phase with the voltage output?
    • TMC4671 - Why does the autotuning with the TMC4671 not seem to work?
    • TMC4671 - Why don’t I get a valid reading from the analog encoder AENC pins?
    • TMC4671 - Why is the motor not reaching the specified target speed?
    • TMC4671 - Why is the motor not turning?
    • TMC4671+TMC6100-BOB - Why is the motor not running in open loop using the wizard?
    • USB-2-RTMI - Can't connect to the TMC4671 via RTMI / Failed to load LibFT4222.dll?
    • USB-2-RTMI - Why does the driver not work after a Windows update?
    • USB-2-RTMI - Why does the TMCL-IDE not see the device?
  • +Technical: FAQ
  • +TMCL: FAQ
  • Topic: FAQ
  • Trinamic Customs: FAQ

TMC4671 - Why is the motor not turning?

If the motor is not turning when using the TMC4671 in your design, it could be that Enable (ENI, pin 55) is not routed. When the ENI pin is not active, you will notice that communication with the chip runs fine but you won’t see a PWM signal and the motor doesn’t turn.

  • Share
  • History
  • More
  • Cancel
 
Related Content
  • TMC4671 undocumented pins
    GOstervall
    The TMC4671 datasheet mentions pins ENI and ENO, in chapter 8. I gathered from the TMC4671_Eval design files as well as the firmware code for the evaluation kit , that ENI probably needs to go high for...
  • TMC4671 - Position Control with Hall Sensors?
    murphdog420
    Hello - We are considering using the TMC4671 for a new BLDC motor control design. My question is whether the TMC4671 can implement position control with only hall sensor inputs, or MUST it have encoder...
  • TMC4671: motor fault detection / safety features
    JKSL
    We are using the TMC4671-LA to control brushed DC motor with an incremental A/B/N as the primary feedback (currently using the TMC4671-EVAL + TMC-UPS-10A70V-EVAL boards to test the design). Is there any...
 
Related Content
  • TMC4671 undocumented pins
    GOstervall
    The TMC4671 datasheet mentions pins ENI and ENO, in chapter 8. I gathered from the TMC4671_Eval design files as well as the firmware code for the evaluation kit , that ENI probably needs to go high for...
  • TMC4671 - Position Control with Hall Sensors?
    murphdog420
    Hello - We are considering using the TMC4671 for a new BLDC motor control design. My question is whether the TMC4671 can implement position control with only hall sensor inputs, or MUST it have encoder...
  • TMC4671: motor fault detection / safety features
    JKSL
    We are using the TMC4671-LA to control brushed DC motor with an incremental A/B/N as the primary feedback (currently using the TMC4671-EVAL + TMC-UPS-10A70V-EVAL boards to test the design). Is there any...