Power Management Fundamentals II Session 5: Deeper Look into Power Protection

    When is the best time to discover your power circuit needs protection? Let's explore the use of some input protection and control options like ideal diodes...
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
      1. Quote of this month: " When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Mature, Not Old! The Longevity of 4 – 20 mA New...
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
    Achieving Power Over Data with RS-485 Transceivers

    By Bryson Barney What if a single wire could carry both energy and information seamlessly—without either getting in the way? The future of connectivity...

     

    ​​Functional Safety: A Driver of “Shift Left”​

    By Richard Obrien The key to faster, safer product development is to start smart - not catch up hard. In this blog, we’ll explore how the "Shift Left...

    Latest Blogs

    • The 5 Advantages of Hardware Fault Tolerance
    • The Power Problem Inside Every AI Breakthrough: Part 1 of 3
    • Simplifying Stability with EVAL-KW4503Z: Part 1 of 3
    • Energy Transfer Considerations in Isolated SMPS: Part 2 of 4
    • Automating LTspice .NOISE Measurements with .STEP and .MEAS Directives: Part 2 of 3
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
Motor Control Hardware Platforms
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Motor Control Hardware Platforms
Motor Control Hardware Platforms
Documents TMC4361A-EVAL - Can I combine this with another motion controller evaluation board?
  • Forums
  • FAQs/ Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADIMonitor: FAQ
  • +Arduino: FAQ
  • +CM40x: FAQ
  • +Code Examples: FAQ
  • +Firmware: FAQ
  • +HPPWM: FAQ
  • +Motor Control: FAQ
  • +Motors: FAQ
  • +PCB Guidelines: FAQ
  • +Platform Schematics: FAQ
  • +Raspberry Pi: FAQ
  • -Specific Products: FAQ
    • Landungsbruecke - Why does the Landungsbruecke show up as “unknown” in the TMCL-IDE?
    • PyTrinamic:How to set global parameter on a Trinamic module using PyTrinamic
    • TMC2130 & TMC5130 - Can I reduce the standby power draw?
    • TMC4361(A) - How can I detect the current state of the HOME reference pin?
    • TMC4361A - How can I use STOPL (respectively STOPR) as home reference?
    • TMC4361A - How do I read out registers from the TMC21x0 through cover datagrams?
    • TMC4361A-EVAL - Can I combine this with another motion controller evaluation board?
    • TMC4361A-EVAL - How should I wire the encoder?
    • TMC4361A-EVAL - Why does the TMCL-IDE not recognize other motor drivers (e.g. TMC2160-EVAL) used with this eval board?
    • TMC4671 - How to enable space vector PWM?
    • TMC4671 - Is it normal to have a current spike if PWM is enabled?
    • TMC4671 - When using the TMC4671 with the TMC6200, why is the current ADC phase not in phase with the voltage output?
    • TMC4671 - Why does the autotuning with the TMC4671 not seem to work?
    • TMC4671 - Why don’t I get a valid reading from the analog encoder AENC pins?
    • TMC4671 - Why is the motor not reaching the specified target speed?
    • TMC4671 - Why is the motor not turning?
    • TMC4671+TMC6100-BOB - Why is the motor not running in open loop using the wizard?
    • USB-2-RTMI - Can't connect to the TMC4671 via RTMI / Failed to load LibFT4222.dll?
    • USB-2-RTMI - Why does the driver not work after a Windows update?
    • USB-2-RTMI - Why does the TMCL-IDE not see the device?
  • +Technical: FAQ
  • +TMCL: FAQ
  • Topic: FAQ
  • Trinamic Customs: FAQ

TMC4361A-EVAL - Can I combine this with another motion controller evaluation board?

Revision Creation Date Revision Author
Current Revision 28 Jul 2023 4:20 PM stephenv
  • View current version