Below is a code snippet showing how to use High Precision PWM (HPPWM) for 3 phase PWM.
HPPWM relies on an internal PLL that multiplies the system clock (SCLK) by a factor of 4. Before enabling HPPWM, make sure SCLK is within the range of 60MHz to 100MHz or the internal PLL will not work.
void Enable_HP_PWM_AC(void){
uint32_t temp_changeMMR;
temp_changeMMR = *pREG_PADS0_PCFG0 + 0x4; // Enable HPPWM in Peripheral Conf. Register
pREG_PADS0_PCFG0 = temp_changeMMR;
temp_changeMMR = *pREG_PWM0_CHANCFG + 0x101010; // Enable HP on phase A+B+C
*pREG_PWM0_CHANCFG = temp_changeMMR;
if (*pREG_PWM0_STAT & 0x80000000){ // Check if HPPWM Ready
{printf("AC High Precision On\n");
}
To set high-precision duty-cycle, use PWM_xH_DUTY0 which holds both the "regular" duty-cycle (PWM_AH0) as well as the HP duty-cycle (PWM_AH0_HP). PWM_AH0 is at [31:16], PWM_AH0_HP is at [15:14].
bits [15:8] of PWM_xH_DUTY0 form the decimal part of a non-integer, fixed-point duty cycle value in Q15.8 format. The lowest bits are ignored. In this example, "regular" duty-cycle is set to 0xAAAA and HP duty-cycle to 0x2=10b
*pREG_PWM0_AH_DUTY0 = 0xAAAA8000; // 1010 1010 1010 1010 1000 0000 0000 0000
*pREG_PWM0_BH_DUTY0 = 0xAAAA8000;
*pREG_PWM0_CH_DUTY0 = 0xAAAA8000;