It looks like it is not activating the STRONG PD (pull down of 2A) on the High-Side-Gate while the Low-Side-Gate is being pulled high.
The rapid decrease of Phase-Voltage does turn on the High-Side-Mosfet. This can only be seen on Y2 and on none of the other 3 Phases.


Is it a configuration that I am missing? In register mode I have configured the following:
I have set for UVW and Y2:
- ADAPTIVE_MODE: 1
- IGATE_SOURCE: 2
- IGATE_SINK: 2
- T_DRIVE_SOURCE: 0xFF
- T_DRIVE_SINK: 0xFF
- BBM_H: 0
- BBM_L: 0
Additionally:
- MCC_PWM_CONFIG -> Y2_HS_SRC : 0
- MCC_GDRV_HW -> HS_AS_LS_Y2 : 0
Yellow: Phase Voltage
Pink: Low-Side-Gate Voltage (with Miller-Plateau)
Blue: High-Side-Gate Voltage to Gnd
Violet: (Math): High-Side-Gate Voltage