Post Go back to editing

MSCNT at different microstep resolution

Thread Summary

The user observed that the TMC2208 microstep counter (MSCNT) does not reach 0 in 1/4-step mode and other lower resolutions, instead being shifted by half of the microstep interval. The final answer confirms this is intended behavior to center current vectors and reduce heating in low step resolutions. The function cannot be disabled, and it is recommended to use coarser microstepping with MicroPlyer for smoother motor operation.

View FAQ
AI Generated Content
Category: Hardware
Product Number: TMC2208

I am investigating the behavior of the TMC2208 microstep counter (MSCNT) when using different microstep resolutions.

According to the datasheet, MSCNT is a read-only counter, but it does not explain how the valid MSCNT positions relate to the selected MRES.

For example, with MRES = 6 (1/4 microstepping), after power-up or after changing to this resolution, I observe the following sequence when applying STEP pulses:

32, 96, 160, 224, ...

instead of

0, 64, 128, 192, ...

Therefore, MSCNT never reaches 0 in 1/4-step mode.

I also found a reply from Bernhard Dwersteg on EngineerZone stating that full-step positions are at:

MSCNT = 128 + 256 × n

This suggests that the internal microstep positions are intentionally shifted by half of the step interval.

Based on my measurements, I suspect that this rule applies to all microstep resolutions:

Microsteps| Valid MSCNT values

1| 128

2| 64, 192

4| 32, 96, 160, 224

8| 16, 48, 80, ...

16| 8, 24, 40, ...

32| 4, 12, 20, ...

64| 2, 6, 10, ...

128| 1, 3, 5, ...

256| 0, 1, 2, 3, ...

In other words, the valid MSCNT positions appear to be shifted by half of the microstep interval for every MRES except 256 microsteps.

Could someone from Analog Devices confirm whether this is indeed the intended behavior of the Trinamic microstep indexer?

If so, what is the reason for this design? Is it done to center the current vectors within each microstep interval, or is there another explanation?

Finally, is there any supported way (other than generating STEP pulses) to align MSCNT to zero when operating at resolutions lower than 256 microsteps?

Parents
  • Hi,

    you are absolutely right with your findings and conclusions. At reduced microstep rates, the effective vector becomes centered around 0. The idea was to reduce extreme positions in low step resolutions, where only one coil contributes to motor torque resulting in strong heating of this coil and driver power stage. This function cannot be switched off. However, we propose to use coarser microstepping only to fit the controller's capability and keep MicroPlyer on to gain smoothest motor behaviour.

Reply
  • Hi,

    you are absolutely right with your findings and conclusions. At reduced microstep rates, the effective vector becomes centered around 0. The idea was to reduce extreme positions in low step resolutions, where only one coil contributes to motor torque resulting in strong heating of this coil and driver power stage. This function cannot be switched off. However, we propose to use coarser microstepping only to fit the controller's capability and keep MicroPlyer on to gain smoothest motor behaviour.

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.