According to the BOM X301 "Jauch Quartz Q 16,0-JXS32-12-10/15-T1-WA-LF" is used. This is a 16MHz 12pF crystal.

On the evaluation board only 9pF was used for C301 & C302. On our circuit board with slightly shorter traces (less capacitance), the crystal fails to start up using 9pF (works with 18pF).
Are my calculations correct? Has anyone tried to actually use the external oscillator on the evaluation baords?
Is this recommandation correct and a crystal with 9pF would perform better or should we stick to the 12pF crystal?
BR
Gabriel