KCC's Quizzes AQQ306 about a fish stick challenge
1. First the quote of the month: " I am so clever that sometimes I don't understand a single word of what I am saying" - Oscar Wilde
2. New quiz AQQ306 about a fish stick challenge:
Here below is a pseudo fish diagram swimming to the right.
Question
View All
November Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Ever wonder how EMC limits came to be and why they matter? Dive into the interesting bits of EMC limits and levels, then test your knowledge with EMC: The Interesting Bits Quiz.
Read the blog first: EMC Limits and Levels Explained: Well, the Interesting
View All
TMC2590
Last Time Buy
The TMC2590 driver for two-phase stepper motors offers an industry-leading feature set, including high-resolution microstepping, sensorless mechanical...
Datasheet
TMC2590 on Analog.com
Hello,
I am using a TMC2590 to drive a 50 V stepper motor, and the MOSFETs are being switched off due to short‑circuit detection. I have observed that the motor outputs show a voltage difference relative to VS.
Could you please tell me what voltage differential between VS and the motor outputs is required to trigger the short‑circuit detection ?
It is roughly 1V: