Post Go back to editing

dcStep Wizard not showing on TMCL IDE (4.3.0) connected to TMC5130 Eval Board (v1.5) through Landungsbrucke (v3.0)

Category: Software
Product Number: TMC5130

I have TMCL IDE 4.3.0 on my laptop connected via USB to the ADI Trinamics Landungsbrucke v3.0 which is connected to the TMC5130-EVAL v1.5.

The TMC5130 clearly states that the dcStep mode is available for the TMC5130 and I can see the dcStep registers in the register browser. There are also videos available from Trinamics showing how to use the dcStep Wizard with the TMC5130 EVAL so it's quite clear that the Wizard should be available for the board I'm using (TMC5130-EVAL v1.5.).

However, the TMCL-IDE doesn't show the dcStep. It shows stallGuard and coolStep... but not dcStep event though it clearly detects the board:

I can see that the dcStep Wizard is not listed in the plugins list:

but I can't find an option to add it / download it or enabled it.

Any idea what I'm missing to make the TMCL-IDE load the dcStep Wizard?

Thank you for your support, much appreciated!