Hi,
I have a question about the body diode of the FET inside the max22201.
Are there any specified values for reverse current?
KCC's Quizzes AQQ306 about a fish stick challenge
1. First the quote of the month: " I am so clever that sometimes I don't understand a single word of what I am saying" - Oscar Wilde
2. New quiz AQQ306 about a fish stick challenge:
Here below is a pseudo fish diagram swimming to the right.
Question
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
MAX22201
Production
The MAX22201/MAX22202/MAX22207 integrate one
36V, 3.5A peak full bridge capable of driving one brushed
DC motor. The full bridge features very low impedance...
Datasheet
MAX22201 on Analog.com
Hi,
I have a question about the body diode of the FET inside the max22201.
Are there any specified values for reverse current?
jnaso - Moved from Interface and Isolation to Motor Control Hardware Platforms. Post date updated from Wednesday, January 14, 2026 6:59 AM UTC to Thursday, January 22, 2026 4:43 PM UTC to reflect the move.
Hi,
I cannot specifically say for this IC- but I can say generally what we do in our drivers:
The body diodes in all of our drivers are rated for the same current as the power MOSFETs themselves, as they take over part of the current in each cycle. However, body diode forward voltage is high, and therefore they lead to large power losses and conduction time needs to be kept low to avoid overheating. To address this, our power drivers actively switch on the MOSFETs when diode conduction is determined to reduce body diode current.
Hope this helps.
Thank you very much for your detailed explanation.
Your description was very helpful and clarified our understanding well.
We appreciate your support and the time you took to explain this.
Best regards,
Thank you very much for your detailed explanation.
Your description was very helpful and clarified our understanding well.
We appreciate your support and the time you took to explain this.
Best regards,