Post Go back to editing

Unexpected Offset in SPI Encoder Commutation Angle Value Calculation when Absolute Position Overflows

Category: Hardware
Product Number: TMC9660

I was setting up TMC9660 FOC with a BLDC on which an Magnetic Absolute Encoder with SPI is attached (AS5047). I was able to get TMC9660 to access the encoder position through SPI1, and TMC9660 was able to initialize in FOC commutation in 8-SPI Enc mode. But the problem is, when commanding a slow velocity, I got this periodic kick from the motor, which I think is the motor suddenly going to the opposite direction for a short moment, then continuing in the correct direction. I think I managed to locate the problem, that is unexpected behavior in the SPI_ENCODER_COMMUTATION_ANGLE value. I setup the motor to spin at a constant velocity in open loop current mode, and expected this SPI_ENCODER_COMMUTATION_ANGLE value to give me a sawtooth waveform, which it did, but when SPI_ENCODER_POSITION_COUNTER_VALUE overflows, the commutation value jumps up from the expected ramp, then later it jumps back down at a later point. Attached is the plot of both the commutation angle and position value when it happened

Some notes

  • BLDC with 7pole pair
  • Magnetic enc through SPI with 13 bit of resolution per rotation
  • LUT correction enable is set to 0
  • TMC9660-EVAL-STP-EVKIT accessed through TMCL-IDE
  • Nothing is attached to the motor apart from the diametrical magnet. The motor is spinning freely
  • The SPI_ENCODER_OFFSET that was set from the previous FOC Initialization is right now 2057, which is coincidentally the one point when that SPI_ENCODER_COMMUTATION_ANGLE ramp suddenly jumps 

Any ideas to why would this happen is greatly appreciated!

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.