Post Go back to editing

Setup for Breaking during Idle

Category: Hardware
Product Number: TMC2209

I am using multiple TM2209 drivers in my design.  I would like to set up the driver to enable the "break" behavior during Idle.

My questions:

1. Can the driver be able to enable the break if the axis has current torque, or current load applies? For example if my Z axis has 2lbs of load on all the time, can my driver is able to "break" by just setting correct IHOLD?

2. Is there any App Note showing how-to enable the "break" feature?  I tried to set the IHOLD value to different value, but I won't be able to make my motor holding.

  • Thank you for your inquiry. Mentioning  for assistance.

  • 电机控制硬件平台中,若轴已存在当前扭矩或负载,驾驶员能否启用制动取决于系统设计的安全逻辑。通常,现代电动汽车的控制器(如MCU)会通过‌扭矩干预策略‌实现以下功能:
    当检测到驾驶员制动请求时,优先执行再生制动或机械制动。
    若当前扭矩与制动指令冲突,控制器会根据预设算法动态调整输出(如扭矩渐降或直接切断动力)。
    关键保护机制包括:扭矩限制、故障安全模式、多传感器冗余校验。
    结合现有信息的补充 :
    现有信息 12提到,电机控制器通过 矢量控制(FOC) 和 PWM调制 实现扭矩动态调节,且硬件电路包含保护模块(如电流/电压监测、通信交互)。这表明系统具备实时响应制动请求的能力‌‌12。
    信息‌‌3指出,电动卡车控制器设计了‌故障处理策略‌,可推断类似逻辑适用于乘用车制动场景(如扭矩与制动的优先级管理)‌‌3。结论 :驾驶员可以启用制动,但具体行为由控制器的安全算法决定,可能包括扭矩逐步释放或直接中断动力输出。硬件平台通过传感器反馈和通信协议(如CAN总线)确保这一过程的实时性与可靠性

    三江机械公司13791863633

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.