Post Go back to editing

Technical Details Regarding the QBL4208-61-04-013-1K Built-In Encoder

Category: Hardware
Hi everyone. I am an electrical engineering student currently working on a university capstone project related to motor control. Specifically, we are attempting to perform speed control on a BLDC motor, with the aim of sending various parameters (i.e. position, phase currents, phase voltages) to a Raspberry Pi 5 for processing. 
The BLDC we plan on using is the QBL4208-61-04-013-1K, which includes a built-in encoder. This specific BLDC can be found via DigiKey: https://www.digikey.ca/en/products/detail/analog-devices-inc-maxim-integrated/QBL4208-61-04-013-1K/9950761?s=N4IgTCBcDaIIoCEAyAWMAGAHAWgGwEZt0Uj8BmbfAaxAF0BfIA
Additionally, we plan to both drive and control the motor using the TMCM-1640 module, which can be found via DigiKey: https://www.digikey.ca/en/products/detail/analog-devices-inc-maxim-integrated/QBL4208-61-04-013-1K/9950761?s=N4IgTCBcDaIIoCEAyAWMAGAHAWgGwEZt0Uj8BmbfAaxAF0BfIA
Lastly, to interface between the TMCM-1640 board and the BLDC motor, we will make use of the TMCM-1640-CABLE package: https://www.digikey.ca/en/products/detail/analog-devices-inc-maxim-integrated/TMCM-1640-CABLE/4399640
My question is related specifically to connecting the BLDC's encoder to the encoder interface of the TMCM board. The encoder interface on the TMCM board has 5-pins, which include:
  • GND
  • +5V Vcc
  • Encoder A channel
  • Encoder B channel
  • Encoder N channel
However, the BLDC's encoder includes 9 wires that correspond to the following connections:
  • Vcc
  • GND
  • Encoder A+ channel
  • Encoder A- channel
  • Encoder B+ channel
  • Encoder B- channel
  • Encoder Z+ channel
  • Encoder Z- channel
  • Shield 

From what I understand, how the 9 wires of the BLDC encoder connect to the TMCM board will depend on the relationship between the A+ and A- wires. For example, if the A+ and A- channels are with respect to ground, then the A-, B-, and Z- wires of the encoder can be left floating (i.e. not connected to the TMCM board). However, if the A+ and A- channels are with respect to each other – that is, if they are differential pairs – then the A-, B-, and Z- wires should all be shorted to GND on the TMCM board. In both cases, I understand that the "shield" wire should short to GND as well.

My question is two-fold: first, is my understanding of the above connection scheme correct? Second, I would appreciate confirmation on how the BLDC's encoder wires are referenced: are the A+ and A- wires with respect to ground, or are they differential pairs? For convenience, I have attached the pinout of the encoder for both the TMCM board and the BLDC motor to this request ticket.

Any help on this subject matter would be greatly appreciated!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.