Post Go back to editing

MAX22201 V18 Pin (LDO) in Sleep Mode

Category: Hardware
Product Number: MAX22201

During sleep mode, what is the expected value of the V18 pin and the OUT1 / OUT2 pins of the MAX22201.  Does the LDO turn off in sleep mode?  I am reading 0V on the V18 pin (decoupled to ground w/ a 1uF cap) and ~1.76V on the OUT1 / OUT2 pins.  Is that expected?  

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.