Category: Software
Product Number: TMCM6214
Hi,
We are using the TMCM6214 and communicating with it using the PyTrinamic Python library.
We are observing intermittent checksum errors during communication. (Full error below) It generally occurs when we poll the motor driver if we have reached the final position, which we do in a 500ms loop.
Basically we have two questions regarding this:
- Is this expected? I.e., are checksum errors common, or does it indicate a hardware issue?
- If the latter, what steps can we take to troubleshoot the issue? Its connected via USB.
Full error:
File "c:\Users\<redacted>\Desktop\<redacted>\venv\lib\site-packages\pytrinamic\modules\TMCM6214.py", line 103, in get_position_reached
return self.get_axis_parameter(self.AP.PositionReachedFlag)
File "c:\Users\<redacted>\Desktop\<redacted>\venv\lib\site-packages\pytrinamic\features\motor_control_module.py", line 119, in get_axis_parameter
return self._parent.get_axis_parameter(ap_type, self._axis, signed)
File "c:\Users\<redacted>\Desktop\<redacted>\venv\lib\site-packages\pytrinamic\modules\tmcl_module.py", line 84, in get_axis_parameter
return self.connection.get_axis_parameter(ap_type, axis, self.module_id, signed, self.ap_index_bit_width)
File "c:\Users\<redacted>\Desktop\<redacted>\venv\lib\site-packages\pytrinamic\connections\tmcl_interface.py", line 201, in get_axis_parameter
value = self._send_ap_cmd(TMCLCommand.GAP, index, axis, 0, module_id, index_bit_width).value
File "c:\Users\<redacted>\Desktop\<redacted>\venv\lib\site-packages\pytrinamic\connections\tmcl_interface.py", line 197, in _send_ap_cmd
return self.send(cmd, tmcl_type, tmcl_motor, value, module_id)
File "c:\Users\<redacted>\Desktop\<redacted>\venv\lib\site-packages\pytrinamic\connections\tmcl_interface.py", line 130, in send
return self.send_request(request, no_reply=no_reply)
File "c:\Users\<redacted>\Desktop\<redacted>\venv\lib\site-packages\pytrinamic\connections\tmcl_interface.py", line 104, in send_request
self._reply_check(reply)
File "c:\Users\<redacted>\Desktop\<redacted>\venv\lib\site-packages\pytrinamic\connections\serial_tmcl_interface.py", line 81, in _reply_check
raise TMCLReplyChecksumError(reply)
pytrinamic.tmcl.TMCLReplyChecksumError: TMCL_Reply: 00,01,64,06,00000000,6D
TMCL_Reply: 00,01,64,06,00000000,6D