Post Go back to editing

Does anybody have the firmware version 1.08 or older for the Trinamic tmcm-1110 StepRocker

Thread Summary

The user is seeking the hex firmware version 1.08 or older for the Trinamic tmcm-1110 StepRocker, as their script, which includes an encoder and buttons, does not function correctly with firmware version 1.09. The final answer confirms that the firmware is available but directs the user to re-post in the support portal for access.
AI Generated Content
Category: Software

Hello, does anybody have the hex firmware version 1.08 or older for the Trinamic tmcm-1110 StepRocker? I can't find it online but my script doesn't work with the version 1.09 which I have installed on a newer steprocker board. It it is a complex script including an encoder and different buttons and a mode switch and only works completely with fw version 1.08 from the original board. With fw 1.09 the target speed changes if I press the left or right movement button but the actual speed remains zero. If I drive the motor directly in the IDE it works normaly.