Hello,
I would want to monitor the current going through the stepper motor coils driven by a TMC5130A.
My goal is to be able to do predictive maintenance, and monitor if the load torque has suddenly increased.
(1) As I understand, the register MSCURACT can't really be used for that purpose since it only reflects the current value from the Look Up Table. Is my assumption correct ?
(2) I was thinking of using a High Side shunt 10mOhm resistor and a current-sense amplifier, hooked up to the ADC of a microcontroller.
However, I can't tell in the datasheet if the 2 VS pins are tied together in the ICs, or if each pin powers a single coil, and so if it would be relevant to have 2 shunt to measure the coils current.
Are the 2 VS pins tied together in the IC ?