Hi there
When I attempt to connect the USB2RTMI to the laptop, TMCL-IDE said Failed to load LibFT4222.dll.
How could I solve the issue?

Thanks in advance.
Hi there
When I attempt to connect the USB2RTMI to the laptop, TMCL-IDE said Failed to load LibFT4222.dll.
How could I solve the issue?

Thanks in advance.
Update: More success after installing FTDI d2xx drivers. Windows 11 device manager now lists my device under "Universal Serial Bus controllers" as two entries; "FT4222H Interface A" and "FT4222H Interface B". However, TMCL-IDE still produces one "Failed to load LibFT4222.dll" error when I try to launch or if I re-connect my USB-SPI debugger.
Hello, I have the same problem with this. Have tried to install to another PC, no luck. Always show “Failed to load LibFT4222.dll”. Do you have fixed this issued yet.
Yes, I have solved it. I will post the method when I’m available.
Yes, I have solved it. I will post the method when I’m available.
So happy to hear that you have solved this problem. Please help me how to fix it.....if you have time!!! Thank you very much!
Please help me! I am really need to work with TMC4671 for my project. Right now everything is stuck. Open a technical support case at Analog Devices support and no one answer me!! Thank you and Appreciate !!!!
I've got the same issue. I look forward to your solution!
Try to put the 32 bit dll to syswow64, and 64 bit dll to the sys32 folder.