| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. | Open | |
Hello -
We are considering using the TMC4671 for a new BLDC motor control design. My question is whether the TMC4671 can implement position control with only hall sensor inputs, or MUST it have encoder inputs to do position control?
Thank you.
I have used the USB-2-RTMI module and the TMCL-IDE to configure position control with the TMC4671 using only the hall sensors. It appears to operate smoothly, although that may differ for your application.
thank you. what were your settings in TCML-IDE to successfully configure position control? i've been unable to identify the correct register settings
My application is using a BLDC motor, but the following registers would apply to any motor, I believe:
[Selectors]
Register=Value
0x52=5
0x50=12
0x51=12
0x63=3
0x0A=150995200 ---> 0x09000100 U=I1, V=I2, W=I0
thank you!