Post Go back to editing

TMC2240 EVA KIT

Category: Hardware
Product Number: TMC2240

I purchase the TMC2240 EVA KIT and after installing PMCL-IDE software I get : Fount 1 PIDs : VID_2A3C&PID_0700 : Driver not found and the software abort... Have a look to the screenshot.  Thanks for help

Parents Reply Children
  • ah, I see. Sorry for the missunderstanding.

    I don’t understand why this is so complicated : I installed a lot of eval boards without any problem of driver and they still work fine.

    I thought that the Landungsbrücke is detected in the IDE since you said that you already worked with it.

    I doubt that's an issue with the IDE then, have you checked if it is running with newer widows? Win 8 is pretty outdated!

    For testing, I installed the TMCL-IDE on a win11 machine and attached the "Landungsbrücke", it got detected without issue

  • Thanks Fabian,

    I will try with a recent windows version.

    By the way I tried with a rpi pi 5 as followed :

    $ python3 FirmwareUpdate.py LandungsbrueckeV3_v3.09.5.BL.hex

    and get the following returns: 

    pytrinamic - TRINAMIC’s Python Technology Access Package

    Openning hex file (Landun…)

    Connecting

    Switching to bootloader mode

    Reconnecting

    ERROR:root:GetVersion returned invalid answer ()

    Regards

    Alain

  • Hi Fabian,

    I intalled tmcl-ide v3.0.7 and it works fine with my eval kit :

    And may kit is not detected with tmcl-ide v3.9.0 :

    So I think that's an issue with this 3.9.0 version.

    I bought this kit BECAUSE it is specified in the TMC2240 Eval-KIT datasheet last version of TMCL-IDE is supported with windows 8 !

    For several reasons I can't migrate to a recent windows version with this application.

    I'm a bit disapointed ...

    Also with 3.0.7 version I cannot upgrade the firmware and I get the same message than with the previous message :

    Could you help me again (AD seems to not update their Trinamic website correctly) ?

    Regards,

    Alain

  • Hard to say how to tackle this problem.

    Well, that is interesting, but I cannot tell if the TMCL-IDE version is the problem here. That is beyond my scope.
    From your Images:
    The first shows that the LANDUNGSBRUECKE is on firmware version 3.07. And connected via USB
    The last image shows the Landungsbruecke as attached to COM and not the USB port.

    I would suggest connecting it via USB.

    Take a look at the top-mark of the processor chip on the Landungsbruecke.
    If the top-mark is "MK20DN256VLL10", you should use the newest "Small" version of Landungsbruecke firmware (example: LandungsbrueckeSmall_v3.09.2_BL.hex).
    If the top-mark is "MK20DN512VLL10", you should use the non-small version of Landungsbruecke firmware (example: Landungsbruecke_v3.09.2_BL.hex).

    See if you can solve the problem.

  • Hi Fabian,

    After a lot of time I got the hit vith the v3.9.0 :

    So we can close the conversation.

    Best Regards,

    Alain

  • Please describe how you resolved the issue in detail, and mark answers as solutions

    This helps others to find a solution if they have similar problems.

    Best

  • Summary:

    --> Windows 8

    --> Installing TMCL-IDE v3.9.0 --> unable to install driver...

    --> Installing TMCL-IDE v3.0.7 from tmcl-ide.software.informer.com --> install driver and connect USB_com11 --> FirmwareUpdate fails

    --> installing TMCL-IDE v3.9.0 --> fails to connect : wants USB_com18 --> Via Windows Device Manager changing com11 to com18

    --> My Landungsbruecke processor is MK20DN512VLL10

    --> Trying FirmwareUpdate from GitHub --> ONLY 'Landungsbruecke_v3.09.6_BL.hex' works --> Landungsbruecke updated to V3.09

    Everything works fine now !

    By the way I am unable to speed my motor more than 131072pps (HEX'20000') ?!?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.