Hi,
I am looking to design board for driving 5 phase stepper motor with pentagon configuration as shown in below picture. Please suggest suitable driver ICs.
Thank you,
K.Venkatarao.
Hi,
I am looking to design board for driving 5 phase stepper motor with pentagon configuration as shown in below picture. Please suggest suitable driver ICs.
Thank you,
K.Venkatarao.
Hi K.Venkatarao,
I guess you need to let all know the motor specs in order to get help. Is that a 1W motor or a 100kW motor?
Cheers, heke
Hi,
OK. Please find the 5 phase stepper motor spec as mentioned below. I am looking for pre-driver and driver IC for 5 phase pentagon stepper motor operation.
5-Phase Stepping Motor with Frame Size 60 mm.
Maximum Holding Torque (N · m) : 2.1
Holding Torque at Motor Standstill (N · m): 1.1
Rotor Inertia J: (kg · m2): 540 × 10-7
Rated Current (A/Phase): 3.8
Basic Step Angle: 0.72°
Power Supply Input : 24 VDC ± 10% 4.8 A
Thank you in advance,
Venkat.
Hi Venkat,
You could probably use 5 x half-bridge chips and an FPGA or an AD's DSP to cook up a drive.
Found also a paper describing a basic circuit.
https://www.sciencedirect.com/science/article/pii/S235197891830355X
Cheers, heke