Post Go back to editing

MAX22200 Serial-Controlled Solenoid and Motor Driver SPI Communication Problem

Category: Software
Product Number: MAX22200ETJ+
Software Version: stm32h747

Hello,

I am trying to read MAX22200 Serial-Controlled Solenoid and Motor Driver data with spi communication. I ran into a few problems and frankly, I couldn't find many examples on the internet so I wanted to ask here.

When I examined the datasheet, I read that I had to send the Command Register to the sensor first and then write data or read data.

For example, when I energize, I want to read the STATUS Register Address(0x00) data of the sensor. I am sending 0x80 by SDI as Command Register. 

In order to be able to read 32-bit data after the data, I send 0x00 by SDI, since no information is given on the datasheet side, I read 0x00 by SDO.

The question mark point stuck in my head here is actually when I change any bit of the STATUS Register, I still read 0x00.

Topics on my mind,

  •  While the command register is sending 8-bit data, only the CMD pin will be made HIGH-LOW, then it should always stay LOW, right?
  • The bit 0x02 status referred to as STATUS[0:7] is understood as FAULT, but what is the status it returns by default?
  • Can you share sample code that I can review on this topic?

Edit Notes

naming error fixed.
[edited by: aemiroglu at 6:19 AM (GMT -4) on 14 Jul 2023]
Parents
  • I had some difficulties understanding controlling this solenoid driver myself, but I created the following sketch in Arduino and I was able to turn solenoids on and off. It is very basic, and I just created this to make sure I understand the operating sequence. Next, I have to create some functions to clean this up, but I hope this helps to understand the sequence:

    #include <SPI.h>

    #define pin_csb 7 // Change this to your chip select pin
    #define pin_en 8 // Change this to your enable pin
    #define pin_cmd 9 // Change this to your command pin

    byte response;

    void setup() {
    Serial.begin(115200);
    delay(500); // delay required to connect to Serial
    Serial.println("Initiated");

    pinMode(pin_csb, OUTPUT);
    pinMode(pin_en, OUTPUT);
    pinMode(pin_cmd, OUTPUT);

    digitalWrite(pin_csb, HIGH); // Keep CS high till SPI is required (chip select)
    digitalWrite(pin_en, HIGH); // Enable the device
    digitalWrite(pin_cmd, LOW);

    SPI.begin();
    SPI.beginTransaction(SPISettings(5000000, MSBFIRST, SPI_MODE0));

    Serial.print("\nInitiated\nResponse from COMMAND register: ");
    digitalWrite(pin_cmd, HIGH);
    delayMicroseconds(50);
    digitalWrite(pin_csb, LOW);
    response = (SPI.transfer(0x00), BIN); // Read = 0, Status register 0x00, use 8MSB = 0
    digitalWrite(pin_csb, HIGH);
    delayMicroseconds(50);
    digitalWrite(pin_cmd, LOW);
    Serial.println(response, BIN);

    delay(100);

    Serial.print("Response from STATUS register: ");
    digitalWrite(pin_csb, LOW);
    response = SPI.transfer(0x00);
    digitalWrite(pin_csb, HIGH);
    Serial.println(response, BIN); // Read the status register

    Serial.println("\nWrite status register to device activation");
    Serial.print("Response from COMMAND register: ");
    digitalWrite(pin_cmd, HIGH);
    digitalWrite(pin_csb, LOW);
    response = SPI.transfer(0x80); // write = 1, Status register 0x00, use 8MSB = 1
    digitalWrite(pin_csb, HIGH);
    digitalWrite(pin_cmd, LOW);
    Serial.println(response, BIN);

    Serial.print("Response from writting to STATUS register: ");
    digitalWrite(pin_csb, LOW);
    response = SPI.transfer(0x01); // Read the status register
    SPI.transfer(0x00);
    SPI.transfer(0x00);
    SPI.transfer(0x00);
    digitalWrite(pin_csb, HIGH);
    Serial.println(response, BIN);

    delay(100);

    Serial.println("\nRead status register for UVM");
    Serial.print("Response from COMMAND register: ");
    digitalWrite(pin_cmd, HIGH);
    digitalWrite(pin_csb, LOW);
    response = SPI.transfer(0x00); // Read = 0, Status register 0x00, use 8MSB = 0
    digitalWrite(pin_csb, HIGH);
    digitalWrite(pin_cmd, LOW);
    Serial.println(response, BIN);

    Serial.print("Response from STATUS register: ");
    digitalWrite(pin_csb, LOW);
    SPI.transfer(0x00); // Read the status register (32 bits)
    SPI.transfer(0x00); // Read the status register (32 bits)
    SPI.transfer(0x00); // Read the status register (32 bits)
    response = SPI.transfer(0x00); // Read the status register (32 bits), and safe status
    digitalWrite(pin_csb, HIGH);
    Serial.println(response, BIN);

    delay(100);

    Serial.println("\nRead again status register to clear UVM");
    Serial.print("Response from COMMAND register: ");
    digitalWrite(pin_cmd, HIGH);
    digitalWrite(pin_csb, LOW);
    response = SPI.transfer(0x00); // Read = 0, Status register 0x00, use 8MSB = 0
    digitalWrite(pin_csb, HIGH);
    digitalWrite(pin_cmd, LOW);
    Serial.println(response, BIN);

    Serial.print("Response from STATUS register: ");
    digitalWrite(pin_csb, LOW);
    SPI.transfer(0x00); // Read the status register (32 bits)
    SPI.transfer(0x00); // Read the status register (32 bits)
    SPI.transfer(0x00); // Read the status register (32 bits)
    response = SPI.transfer(0x00); // Read the status register (32 bits), and safe status
    digitalWrite(pin_csb, HIGH);
    Serial.println(response, BIN);
    }

    void loop() {
    delay(1000);

    Serial.println("\nTurn on the solenoid on channel 0&1");
    Serial.print("Response from COMMAND register: ");
    digitalWrite(pin_cmd, HIGH);
    digitalWrite(pin_csb, LOW);
    response = SPI.transfer(0x80); // write = 1, Status register 0x00, use 8MSB = 0
    digitalWrite(pin_csb, HIGH);
    digitalWrite(pin_cmd, LOW);
    Serial.println(response, BIN);

    Serial.print("Response from STATUS register: ");
    digitalWrite(pin_csb, LOW);
    SPI.transfer(0x01); // Write the status register active
    SPI.transfer(0x00); // Read the status register
    SPI.transfer(0x00); // Read the status register
    response = SPI.transfer(0x03); // Write the status register with Channel 0&1
    digitalWrite(pin_csb, HIGH);
    Serial.println(response, BIN);

    delay(1000);

    Serial.println("\nTurn off the solenoid on channel 0&1");
    Serial.print("Response from COMMAND register: ");
    digitalWrite(pin_cmd, HIGH);
    digitalWrite(pin_csb, LOW);
    response = SPI.transfer(0x80); // write = 1, Status register 0x00, use 8MSB = 0
    digitalWrite(pin_csb, HIGH);
    digitalWrite(pin_cmd, LOW);
    Serial.println(response, BIN);

    Serial.print("Response from STATUS register: ");
    digitalWrite(pin_csb, LOW);
    SPI.transfer(0x01); // Write the status register with active
    SPI.transfer(0x00);
    SPI.transfer(0x00);
    response = SPI.transfer(0x00); // Write the status register with 0 to turn off all channels
    digitalWrite(pin_csb, HIGH);
    Serial.println(response, BIN);
    }

  • Have you managed to get proper return values from the MAX chip? I'm using an stm32 controller and can also turn channels on and off but can't seem to get real return values. I also just tried your arduino sketch since I had an ESP32 board here but then I also only get a UVM flag at start and aftere that only zeroes or ffff.

    Regards

    Lars

Reply
  • Have you managed to get proper return values from the MAX chip? I'm using an stm32 controller and can also turn channels on and off but can't seem to get real return values. I also just tried your arduino sketch since I had an ESP32 board here but then I also only get a UVM flag at start and aftere that only zeroes or ffff.

    Regards

    Lars

Children