Version 4 SHEET 1 2956 904 WIRE 400 64 288 64 WIRE 672 64 624 64 WIRE 1008 64 672 64 WIRE 288 80 288 64 WIRE 1008 128 1008 64 WIRE 400 144 352 144 WIRE 704 144 624 144 WIRE 864 144 704 144 WIRE 704 160 704 144 WIRE 288 176 288 160 WIRE 352 176 352 144 WIRE 864 176 864 144 WIRE 240 224 208 224 WIRE 352 224 320 224 WIRE 400 224 352 224 WIRE 656 224 624 224 WIRE 208 256 208 224 WIRE 656 256 656 224 WIRE 704 256 704 240 WIRE 704 256 656 256 WIRE 352 272 352 224 WIRE 704 272 704 256 WIRE 864 288 864 256 WIRE 1008 288 1008 208 WIRE 208 368 208 336 WIRE 352 368 352 352 WIRE 704 368 704 352 FLAG 352 176 0 FLAG 704 368 0 FLAG 672 64 VOUT FLAG 864 288 0 FLAG 352 368 0 FLAG 288 176 0 FLAG 208 368 0 FLAG 1008 288 0 SYMBOL res 336 256 R0 SYMATTR InstName RSET SYMATTR Value 10.2 SYMBOL res 688 144 R0 SYMATTR InstName R1 SYMATTR Value 976k SYMBOL res 688 256 R0 SYMATTR InstName R2 SYMATTR Value 102k SYMBOL voltage 864 160 R0 SYMATTR InstName V+ SYMATTR Value 5.0 SYMBOL SpecialFunctions\\LTC6993-1 512 144 R0 SYMATTR InstName U1 SYMBOL res 336 208 R90 WINDOW 0 -2 125 VBottom 2 WINDOW 3 32 56 VTop 2 SYMATTR InstName RVCO SYMATTR Value 10.2 SYMBOL voltage 208 240 R0 WINDOW 123 0 0 Left 2 WINDOW 39 0 0 Left 2 WINDOW 3 24 96 Invisible 2 WINDOW 0 40 58 Left 2 SYMATTR Value 0.5 SYMATTR InstName VC SYMBOL voltage 288 64 R0 WINDOW 123 0 0 Left 2 WINDOW 39 0 0 Left 2 WINDOW 3 24 96 Invisible 2 WINDOW 0 41 39 Left 2 SYMATTR Value PWL(0 0.00 9.0m 0 10m 5 11m 0 19m 0 20m 5 21m 0) SYMATTR InstName TRIG1 SYMBOL res 992 112 R0 SYMATTR InstName R3 SYMATTR Value 1k TEXT 480 304 Left 2 !.tran 50m TEXT -272 40 Left 2 ;Ideal TEXT -88 40 Left 2 ;Actual TEXT -448 80 Left 2 ;TPULSE TEXT -272 80 Left 2 ;1.00m to 10.0m TEXT -88 80 Left 2 ; to TEXT -448 120 Left 2 ;VC TEXT -272 120 Left 2 ;0.00 to 1.00 TEXT -88 120 Left 2 ;0.00 to 1.00 TEXT -448 152 Left 2 ;RSET TEXT -88 152 Left 2 ;10.2 TEXT -448 184 Left 2 ;RVCO TEXT -88 184 Left 2 ;10.2 TEXT -448 224 Left 2 ;DIVCODE TEXT -88 224 Left 2 ;NaN TEXT -448 256 Left 2 ;NDIV TEXT -88 256 Left 2 ;NaN TEXT -448 288 Left 2 ;FMASTER TEXT -88 288 Left 2 ; to Hz TEXT -448 328 Left 2 ;ISET TEXT -88 328 Left 2 ;98.0m to 196mA TEXT -448 360 Left 2 ;TSTARTUP TEXT -88 360 Left 2 ; to s TEXT 608 672 Left 2 ;LINEAR TECHNOLOGY CORPORATION TEXT 608 720 Left 2 ;LTC6993 Low Frequency Silicon Oscillator TEXT 608 840 Left 1 ;Generated By LTC6993 Web Tool\nTue Jun 09 2020 15:07:11 GMT+0200 (Mitteleuropäische Sommerzeit)\nCopyright (C) 2020 Linear Technology Corporation TEXT 128 672 Left 2 ;CUSTOMER NOTICE TEXT 128 704 Left 1 ;If a symbol is not found, please update the symbols by selecting\nthe Sync Release command from the Tools menu in the Windows\nversion, or by clicking the Model Update button in the Operation\nTab in the Control Panel in the Mac version.\nIt remains the customer's responsibility to verify proper and\nreliable operation in the actual application. Component\nsubstitution and printed circuit board layout may significantly\naffect circuit performance or reliability.\nContact your local sales representative for assistance. TEXT -496 672 Left 2 ;INSTRUCTIONS TEXT -496 704 Left 2 ;Run the transient simulation, then plot VOUT and VCO\nto verify the the frequency.\n TEXT 208 480 Left 2 ;The LTC6993-1/ LTC6993-3 will ignore additional trigger inputs \nuntil the output pulse has terminated. TEXT 1168 -176 Left 2 ;we are developing a driver stage for feeder. ( device: 230 VAC;50 Hz )\nthis should be performed by cutting a leading or trailing edge of the ac power.\nFurthermore a TRIAC and the zero detect signal is used. The procedure ist as following:\nThe zero signal is detected => the voltage controlled PWM will be started to fire the triac.\nI have done a LTSPICE simulation with the LTC6993-1 (non retriggered ) and expect the start of tehe PWM after the rising edge of the zerro detect signal.\nBut the signal is not as expected. !\nkinds regard \n bernd\nis there a possibility to send the LTSPICE asc file LINE Normal 320 144 320 144 2 LINE Normal 336 272 336 272 2 LINE Normal -270 58 -170 58 LINE Normal -90 58 10 58 LINE Normal 160 144 160 144 2 RECTANGLE Normal -500 -228 1100 900 RECTANGLE Normal 1100 820 596 692 RECTANGLE Normal 1100 692 596 644 RECTANGLE Normal 596 900 108 644 RECTANGLE Normal 108 900 -500 644we are developing a driver stage for feeder. ( device: 230 VAC;50 Hz )
this should be performed by cutting a leading or trailing edge of the ac power.
Furthermore a TRIAC and the zero detect signal is used. The procedure ist as following:
The zero signal is detected => the voltage controlled PWM will be started to fire the triac.
I have done a LTSPICE simulation with the LTC6993-1 (non retriggered ) and expect the start of tehe PWM after the rising edge of the zerro detect signal.
But the signal is not as expected. !
kinds regard
bernd
attached the LTSPICE asc file