Hi,
I am using the AD2S1210 for the velocity of a BLDC and position of the stepper motor, I am using the SPI communication here I am getting the position register value is varying from 0-0x7FFF for 0-180 degrees and position register value is becoming the zero and varying from 0-0x7FFF for remaining 180 degrees (180 -360) is these values are correct or not.
Here I am using the 8-bit mode for SPI communication and resolution 10-bit, Excitation frequency as 10KHz. Please help me for calculating the speed also.
Looking forward to your reply,
Regards,
B.Durga sivarkishna