Article How do I implement Timer Interrupt in TMCL?

This program below demonstrates how to use the timer interrupt.

To use this program, connect LEDs to OUT_0 and OUT_1. The LED at port OUT_1 is toggling at 2 Hz using the WAIT command. Connect a LED to port OUT_0. This LED connected to OUT_0 will be toggling at 1 Hz using the timer interrupt.

Before use: Restore Factory Defaults.

        // *** Interrupt initialization *** // 
VECT 0, Timer0Irq //defines the interrupt vector for the timer 0 interrupt
SGP 0, 3, 1000 //configure the timer interrupt: set its period to 1000ms
EI 0 //enable timer interrupt
EI 255 //globally switch on interrupt processing

// *** Main Loop *** //
loop:
SIO 1, 2, 1 //switch OUT_1 high
WAIT TICKS, 0, 50 //wait 0.5 seconds. 50 * 10ms
SIO 1, 2, 0 //switch OUT_1 low
WAIT TICKS, 0, 50 //wait 0.5 seconds. 50 * 10ms
JA loop //jump to loop
// *** Interrupt routine *** //
Timer0Irq:
GIO 0, 2 //check if OUT_0 is high
JC NZ, Out0Off //jump to Out0off if high
SIO 0, 2, 1 //switch OUT_0 high
RETI //end of interrupt
Out0Off:
SIO 0, 2, 0 //switch OUT_0 low
RETI //end of interrupt

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.