Article How do I set an interrupt input change?

The short program below demonstrates how to set the interrupt on an input change in TMCL. The behavior of this program is the same as EX0008. Depending on the status of Port IN_0, motor 0 turns right (IN_0 = 0) or left (IN_0 = 1).

Before use: Restore Factory Defaults.

// *** Values that have to be adapted *** // 
amax = 1000 //max. acceleration (0 ... 2047)
vmax = 2000 //max. speed (0 ... 2047)
cmax = 100 //max. current (0 ... 255)

// *** Initialization / Set up axis parameter *** //
SAP 5, 0, amax //set max. acceleration
SAP 6, 0, cmax //set max. current

// *** Interrupt initialization *** //
VECT 39, changeRotation //define the interrupt vector for input change 0 interrupt (IN_0)
SGP 39, 3, 3 //configure interrupt to trigger on both edge of input 0 (0=off,1=low-high,2=high-low,3=both)
EI 39 //enable input change 0 interrupt (IN_0)
EI 255 //globally switch on interrupt processing

// *** Main Loop *** //
loop: //infinite loop
JA loop //jump to loop

changeRotation:
GIO 0, 0 //read IN_0
COMP 0 //compare with 0
JC EQ, turnRight //if equal jump to turn right R
ROL 0, vmax //if not equal turn left at vmax
RETI //end of interrupt
turnRight:
ROR 0, vmax //turn right at vmax
RETI //end of interrupt

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.