Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp Open Loop Gain and LTspice

      A kind proposal from Al Butvidas 1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Understanding Voltage Domain Isolation in Field-Bus...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

EngineerZone
EngineerZone
Ultra Low Power Microcontrollers
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Ultra Low Power Microcontrollers
  • Processors & Microcontrollers
Ultra Low Power Microcontrollers
Documents Handling CRC in an IAR project for ADuCM302x
  • Q&A
  • File Uploads
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADuCM3029: FAQ
  • -ADUCM302x: FAQ
    • ADuCM302x Register List - MMR Address Map
    • "What is the highest UART baud rate that can be used while ensuring reliable communication?"
    • "Where can I find documentation related to ADuCM302x or ADuCM4050 software drivers (DFP, BSP)?"
    • "Why does my application run in DEBUG mode but not in RELEASE mode?"
    • Can I disable HFOSC ?
    • Can the part enter Hibernate/Shutdown with HFXTAL as root clock source?
    • Handling CRC in an IAR project for ADuCM302x
  • +ADuCM4050: FAQ
  • +RX FIFO: FAQ
  • +ADuCM4x50: FAQ

Handling CRC in an IAR project for ADuCM302x

There is a "Checksum" tab under the "Linker" settings in the IAR project options, which can be used to generate the CRC of the user application code. In order to store the correct CRC, the following settings must be used:

1. Check “Fill unused code memory”

2. Set the “Fill pattern -> End address” to 0x7FB (changes depending on page number, default is 0)

3. Check “Generate checksum”

4. Select “4 bytes” from the “Checksum size” pull - down

5. Set “Alignment” to 4(bytes)

6. Select “CRC32” from the “Algorithm” pull - down

7. Set the “Initial value” to 0xFFFFFFFF and uncheck “Use as input”

8. Select “32 - bit” from the “Checksum unit size” pull - down

There is a "Extra Options" tab under the "Linker" settings in the IAR project options, which needs to be configured as

1. Check “Use command line options”

2. Use "--keep __checksum" as first line in command line options box

Tags: aducm3xxx aducm302x