Power Management Fundamentals II Session 6: Key Layout Considerations for Power

    Understand the physics of printed circuit boards to manage large changes in current or voltage. See how layout tweaks can make big improvements for your...
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
    • Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads
    • Understanding and Selecting RF Low Noise Amplifiers for Instrumentation, Phased Array and General Purpose Applications
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
      1. Quote of this month: " When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Mature, Not Old! The Longevity of 4 – 20 mA New...
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
    Taming the Chaos: Correlated and Uncorrelated Sources in LTspice .NOISE Simulations: Part 3 of 3

    Noise analysis of a circuit requires tracking several things simultaneously: each noise source, how those noise sources are shaped by the circuit, and...

     

    ​​Where Errors Lurk in the GMSL Signal Chain​

    Whether you're debugging a stubborn camera link or designing a robust system from scratch, knowing where errors hide is half the battle. GMSL provides...

    Latest Blogs

    • Achieving Power Over Data with RS-485 Transceivers
    • ​​Functional Safety: A Driver of “Shift Left”​
    • The 5 Advantages of Hardware Fault Tolerance
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
Ultra Low Power Microcontrollers
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Ultra Low Power Microcontrollers
  • Processors & Microcontrollers
Ultra Low Power Microcontrollers
Documents How to - ADuCM3029 with simple and free Open Source Tools?
  • Forums
  • File Uploads
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • +Documents
  • -ADuCM3029: FAQ
    • ADuCM3029/ADuCM3027 MMR Address Map
    • ADuCM302x Register List - MMR Address Map
    • How to - ADuCM3029 with simple and free Open Source Tools?
    • How to Interface ADuCM3029 and ADuCM4050 with ICE-2000
    • How-To use EVAL-ADICUP3029 / EV-COG-AD3029 with emIDE
  • +ADUCM302x: FAQ
  • +ADuCM4050: FAQ
  • +RX FIFO: FAQ
  • +ADuCM4x50: FAQ

How to - ADuCM3029 with simple and free Open Source Tools?

For those who are interested in Bare Metal Programming - as myself - or simply starting to develop Embedded Applications, in my opinion the high sophisticated tool-chains (i.e. Eclipse based) and commercial available tool-chains (I.e. IAR EWARM or Keil ARM) are sometimes more complicated to use than simple tools available for free and Open Source.

Also we get from time to time questions on how to get started with free of charge tools without limitations - i.e. code-size or time-limits.

So I made some investigations on Windows and Linux about IDEs and tools to be used with our Analog Microcontrollers or CM4xx Mixed-Signal Control Processors, which are based on ARM cores. Most of the Evaluation-Kits we provide come with J-Link Debugger-Dongles for programming and debugging, so the main interest was about Software which works with those.

On Windows I discovered already some time ago emIDE - this is a lightweight simple to use IDE with some basic Bare Metal Code examples and some nice features. In another thread I attached a very, very basic example project for the ADuCM3029 done on emIDE - Not working after HW-Reset or Power-Cycle.

Also there are other tool-chains which can be used for this purpose available for Windows, i.e. Code::Blocks (emIDE is based on this), CodeLite, emBlocks (also based on Code::Blocks) and maybe more.

Nowadays we also get more and more questions about tools running on Linux systems.
I used Code::Blocks now for test on Linux to do an bit more enhance version of the ADuCM3029 example project. This is attached here with a more comprehensive header-file, linker-control-file and Interrupt-Vectors for all peripherals included in the startup.s file.

In all cases the key is the GDB-server support for the J-Link Debugger-Dongles from Segger.
Other tool-chains besides Code::Blocks are also CodeLite and a complete different, but very interesting approach ddd (DataDisplayDebugger) working perfectly on Linux systems.
All those are free of charge and in combination with the GNU C Compilers for ARM have no limitations.

The J-Link GDB-server is also available for small, lightweight and low-power ARM-Linux-systems like a Raspberry Pi.
I tried running Code::Blocks on a Raspberry PI 2 and below a screen-shot where I did develop the attached example project on an Orange PI Plus - which has a quad-core running up to 1.56GHz. With a Debian 8 Jessie Linux Distribution it works reliable fast and can be used to develop Embedded Applications for Analog Microcontrollers like the ADuCM3029.

Attachments:
ez.analog.com/.../2262.ADuCM3029_5F00_Int_5F00_Blink.tar.gz
Tags: microcontrollers aducm302x Precision Microcontrollers aducm3029
  • Share
  • History
  • More