Hi Team,
I am using the MAX32675 EV-KIT Rev-D and trying to run the SPI1 Master example from the MSDK. The example is not working on the evaluation board, so I need clarification on the hardware and pin configuration.
Could you please confirm the following:
-
Which pins are officially used for SPI1 on the MAX32675 EV-KIT Rev-D?
(MISO, MOSI, SCK, SS0) -
Are there any jumper settings required on the EV-KIT to enable SPI1?
-
Do the SPI examples in the MSDK need any code changes for EV-KIT Rev-D?
Or should the example work with the default pin configuration? -
Is SPI1A (P0.14, P0.15, P0.16, P0.17) supported on this EV-KIT revision?
-
Which pin mapping should we connect to an external SPI device on EV-KIT Rev-D?
I am unable to get the SPI1 example working, so your guidance on correct pin mapping, jumpers, and configuration will be very helpful.