Post Go back to editing

Programming MAX96717f + MAX96714F once

Category: Hardware
Product Number: MAX96717F

HI,

I am using SerDes MAX96717F Ser and MAX96714F Des (MAXIM INTEGRATED) along with raspberry pi 4 to get the output of Raspi Camera on RPi4.

1: The pipeline has been generated using the GMSL gui through script generation.

2: Once cpp file is loaded, i am able to get the display at the Rpi4.

The issue is whenever i power cycle the boards. I need to load the script again to get the output.

How can i program it for once and use it even after power cycle?

Any leads?

Parents Reply Children
No Data