Post Go back to editing

Programming the device.

Category: Software
Product Number: MAX28200
Software Version: MAX28200 EV Kit 1.6.0

Hi there. I'm trying to program the MAX28200 Microcontroller EV Kit using the MAX28200 EV Kit v1.6.0 software. I have managed to write a small program that ouputs to PO[2] and created a hex file of that program. However, when I click on the Program\Verify button, the MAX28200 EV Kit v1.6.0 program runs continously and nothing happens; like an infinite loop. A red light appears on the DS9481P circuit board and that is all. I can close the program and normally afterwards I press the reset button on the EV Kit which gets rid of the red light on the DS9481P circuit board.

How can I fix this problem?

Thanks.