Post Go back to editing

How to convert CN0510 sample code to a CCES project?

Category: Software
Product Number: cn0510
Software Version: 2.12.0

Good evening,

I see CCES as the recommended toolchain for this ADICUP3029

https://wiki.analog.com/resources/eval/user-guides/eval-adicup3029

But then the Battery Impedance example (which is what I'm trying to use), directs to here

https://wiki.analog.com/resources/eval/user-guides/circuits-from-the-lab/cn0510

Which doesn't mention CCES.  So far, I've been able to get the sample code working on keil. But I primarily use linux.  So if I can use CCES for this project, that'd be my preference (even better if I could just use cli and cmake, but I don't see that as an option anywhere).

I was able to make a couple of the CCES ADICUP3029 examples build and run. 

But when I try to import the AD5940 examples, CCES recognizes them as projects

but apparently not the right kind of project, because there's no option to build or run.

  I guess this means that CCES isn't recognizing it as a C/C++ or CrossCore project?  If so, what tweaks do I need to make in order to successfully build and run this example on CCES?

Thank you, take care

Thread Notes