Post Go back to editing

Hello AD, My EVALADICUP3029 is not being detected by PC when i connect via USB to MicroUSB. It shows as "MAINTAINECE" and it doesn't in Device Manager as well.

Product Number: EVALADICUP3029
Software Version: KEIL IDE 5

Hello AD,
My EVALADICUP3029 is not being detected by PC when i connect via USB to MicroUSB.
It shows as "MAINTAINECE" and it doesn't in Device Manager as well.
I installed Cross Core Serial Programmer and but it doesn't show up in that as well.


Attached screenshots for your reference.


Regards
Amar

Parents
  • FormerMember
    0 FormerMember
on Aug 1, 2023 10:26 AM

Hi Amar,

Not 100% sure, but this looks like it could be a driver issue between the EAVL-ADICUP3029 board and the PC you are using.  Could you try downloading and updating the driver, here is a link I've used in the past that has solved this problem for me Windows serial configuration - Handbook | Mbed .  Let me know if this helps.

Cheers,

Brandon

  • Hello Brandon,

    Reinstalling the Mbed driver on my PC did not help.
    I have an other EVAL ADICUP3029 board that came along with EVALAD5940ELCZ and that is working fine.
    So i do not think my PC has driver issue.
    Kindly look into it.

    Regards

    Amar

  • Reply Children
    No Data