Post Go back to editing

ADUCM355 Fifo threshold

Thread Summary

The user encountered an issue with the ADuCM355 where setting the M355FifoThresh to values less than 7 in the AD5940Main.c file results in the UART outputting more measurements than expected. The final answer explains that this is due to multiple interrupts occurring before the sleep state is unlocked in AppAMPISR(), causing some interrupts to be missed. Values >=7 work correctly as they allow sufficient time for the interrupts to be serviced.
AI Generated Content
Category: Software
Product Number: EVAL-ADuCM355QSPZ
Software Version: Keil uVision V5.37

Hello,

I have tried out the example M355_ECSns_SingleWE, which is working fine so far. Now i want to change the number of measurements, so i changed the pAmpCfg->M355FifoThresh = 10; in the AD5940Main.c. A threshold value of 8 or 9 works as expected, but when I change the threshold to pAmpCfg->M355FifoThresh = 3 it will send this to UART:

Hello AD5940-Build Time:13:52:47
This ADuCM355!
Note: Current Silicon is S2
AD5940LIB Version:v0.2.0
Freq:32097.126953
Calibrated Rtia = 106275.500000
Index 0:, 0.064 , uA
Index 1:, 0.064 , uA
Index 2:, 0.064 , uA
Index 0:, 0.064 , uA
Index 1:, 0.064 , uA
Index 2:, 0.064 , uA
Index 3:, 0.064 , uA
Index 4:, 0.064 , uA
Index 5:, 0.064 , uA
Index 6:, 0.064 , uA

Why does it correctly send the Index 0,1,2, as I chose 3 as threshold, but then immediately send another 7 values? I recognized, that this would happen also with other thresholds, for example 4 and it will send another 6 values afterwards. So always summing up to 10, I think.

I would appreciate any help, thank you.

Kind regards, Alexander