Post Go back to editing

I2C_ADUCM_3029_bug

Hello,

When I try to transmit a buffer to an I2C slave through uart a hard fault is generated (BusFault_Handler B BusFault_Handler

ADI_HAL_STATUS_t I2C_Transmit(uint16_t address,uint8_t *pData, uint8_t size)
{
/* set slave address to ADPD105 default 0x64 without read0/write1 bits */
if (adi_i2c_SetSlaveAddress(i2CDevice, address)) // bottom-end
{
//DEBUG_MESSAGE("couldn't set slave device address");
}
tran.pPrologue=pData; /*!< Prologue pointer. */
tran.nPrologueSize=1; /*!< Prologue byte count. */
tran.pData=pData+1; /*!< Data pointer. */
tran.nDataSize=size-1; /*!< Data byte count. */
/* false to write*/
tran.bReadNotWrite=false; /*!< Read/write flag. */
tran.bRepeatStart=false; /*!< Repeat start flag. */
ADI_HAL_STATUS_t ret;
adi_i2c_ReadWrite(i2CDevice,&tran,&hwErrors) //bug
return ret;
}

Executing the code step by step shows that the  hard fault is generated when waiting I2C_BUSY in the adi_i2c.c module

static void submitTransaction(ADI_I2C_HANDLE const hDevice, ADI_I2C_TRANSACTION* const pTransaction) {

/* reset internal return code */
hDevice->result = ADI_I2C_SUCCESS;

/* reset hardware error code */
hDevice->hwErrors = ADI_I2C_HW_ERROR_NONE;

/* wait for HW to be ready */
while (I2C_BUSY) {
;
}

Could  you define what is the cause of the hardfault?

Parents Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.