Locale Icon
English
EngineerZone
EngineerZone
Precision Microcontrollers
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
    Accelerate RF Subsystem Integration with COTS SoMs and Phased Array Solutions. As building a subsystem from early prototype to full deployment is never...
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
      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Calibration Implementation Techniques for Multichannel Phased Array Subsystems

    Learn about phase-calibration techniques used for characterizing a 16 transmit and 16 receive X-band phased array subsystem based on a mixed-signal front...

Precision Microcontrollers
  • Processors & Microcontrollers
Precision Microcontrollers
Documents Can the MAX32664A algorithm compensate for future sensor degradation or smartphone “aging”?
  • Q&A
  • Docs/FAQs
  • File Uploads
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADuCM Cortex-M3: FAQ
  • +ADuCM310 FAQ:
  • +Aducm320: FAQ
  • +ADuCM350: FAQ
  • +ADuCM355: FAQ
  • +ADuCM360: FAQ
  • +ADuCM361: FAQ
  • +ADuCM362 FAQ:
  • +ADuCRF101: FAQ
  • +Bio-Impedance & ECG Measurement Solution: FAQ
  • +CN0300: FAQ
  • +Continuously Amperometric Measurement: FAQ
  • Do we need new Maxim supplied algorithms for the MAX32664, as I assume that the ones provided for the MAXREFDES101 do not support SpO2?
  • +EVAL-ADUCRF101MKxZ FAQ:
  • +MAX32663A: FAQ
  • MAX32664-A HRM & SPO2 FIRMWARE V10.0.0: FAQ
  • +MAX32664GTGA+: FAQ
  • +MAX32664GTGC+: FAQ
  • +MAX32664GTGZ+: FAQ
  • -MAX32664GWEA+: FAQ
    • Can the MAX32664A algorithm compensate for future sensor degradation or smartphone “aging”?
    • Does the MAX32664 provide the raw sensor data, in addition to the processed sensor data?
    • Does the MAX32664 support field updates?
    • Does the MAX32664 use SPI?
    • I am observing unexpected results when pulling data from a smart sensor FIFO at high rates. What is going on?
    • Is the KX-122 accelerometer in the MAXREFDES101 configured to 2g, 4g or 8g range?
    • Is there an EV Kit for the MAX32664?
    • Is version A of the MAX32664 Sensor Hub storing data into the FIFO at 100Hz or sampling the sensors at 100Hz?
    • MAX32664 Solder ball material?
    • The MAX32664GWEA, B, C, D does not go to application mode when using the RST_N and MFIO lines. The device mode returns bootloader mode even after waiting 1 sec. What might be wrong?
    • What is the difference between the MAX32664A and the MAX32664B?
    • What is the MAX32664?
    • What is the MAX32664A?
    • What is the MAX32664B?
    • Which accelerometer is on the MAXREFDES220?
    • Which biometric parameters does the MAX32664 (A) measure?
    • Which optical sensors can be used with the MAX32664 (A)?
    • Which optical sensors can be used with the MAX32664 (B)?
  • +MAX32664GWEB+: FAQ
  • +MAX32664GWEC+: FAQ
  • +MAX32664GWED+T: FAQ
  • +MAX32674C: FAQ

Can the MAX32664A algorithm compensate for future sensor degradation or smartphone “aging”?

The answer is yes, and more:

The MAX32664A Algorithm has an Automated-Gain-Control (AGC) to adjust LED power and/or AFE acquisition durations to get the optimum signal levels. This would provide adequate compensation for sensor (Photo Detector) sensitivity or LED drive parameters due to age or part-to-part variations.

 

Tags: KA-07402 aging degradation algorithm agc sensor automatic gain control smartphone MAX32664GWEA+ MAX32664A Show More