Locale Icon
English
EngineerZone
EngineerZone
Precision Microcontrollers
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
    Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads

    As the Space market evolves and accelerates, mission designers need space-capable electronics that balance performance, reliability, and affordability...
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
    • Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads
    • Understanding and Selecting RF Low Noise Amplifiers for Instrumentation, Phased Array and General Purpose Applications
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
      1. Quote of this month: " When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Mature, Not Old! The Longevity of 4 – 20 mA New...
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
    Taming the AI Power Storm: Part 2 of 3

    Let’s peel back the curtain on how Analog Devices (ADI) is leading the charge, crafting power solutions that not only keep up with AI’s appetite but redefine...

     

    TIA Me Up, But Keep It Stable: Part 2 of 3

    Imagine trying to measure a current so tiny that it’s almost invisible. How is that even possible? How do we even convert that current signal into something...

    Latest Blogs

    • Celebrating Innovation: Top 3 EngineerZone Spotlight Blogs from 2025
    • Transforming Power: Transfer Techniques in SMPS: Part 3 of 4
    • Taming the Chaos: Correlated and Uncorrelated Sources in LTspice .NOISE Simulations: Part 3 of 3
    • ​​Where Errors Lurk in the GMSL Signal Chain​
    • Achieving Power Over Data with RS-485 Transceivers
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
Precision Microcontrollers
  • Processors & Microcontrollers
Precision Microcontrollers
Documents Known Issues for ADuCM350 Silicon and Support Material
  • Q&A
  • Docs/FAQs
  • File Uploads
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADuCM Cortex-M3: FAQ
  • +ADuCM310 FAQ:
  • +Aducm320: FAQ
  • -ADuCM350: FAQ
    • 4Wire-Isolated-Bioimpedance ADuCM350 Connections To Sensor
    • ADUCM350 DESIGN SUPPORT COMMUNITY - INTRO
    • ADuCM350 FAQ DFT / Impedance Measurement
    • ADuCM350 FAQ Debug
    • ADuCM350 FAQ Evaluation Kit Software Platform
    • AFE Transmit Stage
    • ADuCM350 FAQ GPIOs and Pinmuxing
    • ADuCM350 FAQ I2C serial interface
    • ADuCM350 FAQ Operational Supply Range / Power Supplies
    • ADuCM350 FAQ Parallel Display Interface(PDI)
    • ADuCM350 FAQ Power Consumption
    • ADuCM350 FAQ Power Management Unit
    • ADuCM350 FAQ Random Number Generator
    • ADuCM350 FAQ SDK Driver Specific FAQs
    • ADuCM350 FAQ SPI
    • ADuCM350 FAQ Switch Matrix
    • ADuCM350 FAQ System Clocks
    • ADuCM350 FAQ System Integrity
    • ADuCM350 SDK v2.3.0.0 now available
    • Bioimpedance Measurement Using ADuCM350
    • Optimizing RCAL,RTIA,CTIA and DAC voltage of ADuCM350 for 4-Wire Measurement.
    • Potentiostat / Amperometric Measurement Using ADuCM350
    • Unipolar Current Measurement Using ADuCM350
    • Errata for ADuCM350 I2C serial interface
    • FAQ ADuCM350 Embedded Software Development
    • How to get SDK + Eval-ADuCM350EBZ Working together.
    • FAQ for Captouch on ADuCM350
    • Known Issues for ADuCM350 Silicon and Support Material
    • ADuCM350 FAQ ADuCM350 Evaluation Kit
    • ADuCM350 FAQ AFE / ADC Measurement Channel
    • ADuCM350 FAQ AFE Measurement Circuit Impedance Range
    • ADuCM350 FAQ AFE TIA
    • ADuCM350 FAQ AFE Sequencer
    • ADuCM350 FAQ Amperometric Measurement Example
    • ADuCM350 FAQ Calibrate
    • ADuCM350 FAQ CRC accelerator
    • ADuCM350 FAQ GP Timers
    • ADuCM350 FAQ LCD controller
    • New Revision of UG-587 Available
    • ADuCM350 FAQ Potentiostat / Amperometric
    • ADuCM350 FAQ Real Time Clock (RTC)
    • First Steps: Quick Measurement with Eval-ADuCM350 & EKSP Labview GUI
    • ADuCM350 SDK v2.4.0.0 Released!
  • +ADuCM355: FAQ
  • +ADuCM360: FAQ
  • +ADuCM361: FAQ
  • +ADuCM362 FAQ:
  • +ADuCRF101: FAQ
  • +Bio-Impedance & ECG Measurement Solution: FAQ
  • +CN0300: FAQ
  • +Continuously Amperometric Measurement: FAQ
  • Do we need new Maxim supplied algorithms for the MAX32664, as I assume that the ones provided for the MAXREFDES101 do not support SpO2?
  • +EVAL-ADUCRF101MKxZ FAQ:
  • +MAX32663A: FAQ
  • MAX32664-A HRM & SPO2 FIRMWARE V10.0.0: FAQ
  • +MAX32664GTGA+: FAQ
  • +MAX32664GTGC+: FAQ
  • +MAX32664GTGZ+: FAQ
  • +MAX32664GWEA+: FAQ
  • +MAX32664GWEB+: FAQ
  • +MAX32664GWEC+: FAQ
  • +MAX32664GWED+T: FAQ
  • +MAX32674C: FAQ

Known Issues for ADuCM350 Silicon and Support Material

ADuCM350 Known Silicon Issues


ADuCM350 V1.4 silicon will release in March 2016. The change from V1.2 to V1.4 is a minor metal edit to improve the robustness of the high frequency, internal RC oscillator (HFOSC). Both MAN_ID and CHIP_ID information will be updated as part of this change.

Issue Description Workaround(s)
VBACK domain leakage Excessive leakage on VBACK domain when in use as backup supply. No solution available. It is recommended not to use SuperCap/VBACK mode.
UPLL pre-charging requirement UPLL must ne pre-charged before being used. SDK Version 2.4+ includes extra lines of code when using the UPLL to pre-charge the VCO loop.
High frequency crystal (HFXTAL) and duty cycle correction (DCC) block It has been found that when the HFXTAL and DCC block are used as the root clock source, it is sensitive to digital noise. Always use the system PLL (SPLL) as the root clock when the HFXTAL is source.
System PLL and USB PLL (SPLL/UPLL) Status Bit The SPLL/UPLL status bit threshold is too low and can cause the SPLLUNLOCK / UPLLUNLOCK bit to set when it is locked. Use SPLL / UPLL lock bit(s) (SPLLLOCK / UPLLLOCK) to reliably determine when the PLL is locked initially. Do not use SPLLUNLOCK / UPLLUNLOCK bit as a reliable indicator that the PLL has lost lock.



ADuCM350 Datasheet

 

In Rev.A of the ADuCM350 datasheet, there is an error in Figure 31 and Figure 32. For both figures, the Z value is incorrect. It should read:

    Z = 140Ω + 68nF

Also, the Y-axis label should read:

    Number of Measurements

The same corrections apply to both Figure 31 and Figure 32. It should also be noted that the capacitors used for these measurements (including the accuracy measurements in Figures 29 and 30) were COG capacitors with 1% tolerance. This tolerance may cause a slight deviation from the ideal value.

 

 

I2C Block

 

Full I2C errata document available here.

Issue Description Workaround(s)
I2C bus hangs when configured as slave Tx During a read from the master to slave, if the slave’s FIFO is empty, the slave should NACK the master’s request. Then it should release the bus allowing the master to generate a STOP condition. In the case of the slave’s FIFO buffer being empty, if data is loaded when the ninth SCL clock is high, the slave generates an ACK to the master and the MSB of read data is sent on the following SCL positive edge. If the MSB is 0, the SDA line will be held low and the slave will wait for extra SCL clocks to transmit the remaining bits. When this happens, the I2C master detects a NACK and then generates a STOP condition. Master arbitration is lost due to the SDA line being indefinitely low.
  1. Placing valid data in the Slave Tx FIFO.
  2. Set the BUS_CLR_EN bit in the I2CMCON register. If this bit is set, the master will initiate a Bus-Clear operation by sending up to 9 extra SCL cycles.
  3. Set EARLYTXR bit in the I2CSCON register. Setting this bit enables a transmit request just after the positive edge on the SCL line during the read bit transmission.
  4. Resetting the slave interface by disabling/enabling the slave.
I2C master fails to operate when the sum of the values in HIGH and LOW in the I2CDIV register has a value of less than 18 (0x12)

In an attempt to minimize the power consumption of the I2C interface, it may be desirable to set the PCLK frequency to 1MHz and set the SCL frequency to 100kHz. Using the provided formula, this would lead to the following HIGH and LOW values in the I2CDIV register:

HIGH = (REQD_HIGH_TIME / PCLK_PERIOD) – 2

HIGH = ((10us / 2) / 1us) – 2

HIGH = 3

LOW = (REQD_LOW_TIME / PCLK_PERIOD) – 1

LOW = ((10us / 2) / 1us) – 1

LOW = 4

When these values are programmed, the I2C master will not function.

  1. Use the adi_I2C_SetMasterClock() function to set the SCL frequency. Ensure to check for a valid return code.
  2. Do not program values to the HIGH and LOW fields in the I2CDIV register which give a sum of less than 18 (0x12).
I2C slave hangs the I2C bus when clock stretching is enabled

Clock stretching is an I2C feature that allows a slave device to temporarily pause communication by holding SCL low (for example, a slave device receives a READ request from a Master but, its Transmit FIFO is empty).

Clock stretching is enabled setting the STRETCHSCL bit in the I2CSCON register to 1. If this is done on the rising edge of SCL a glitch can occur. Other devices might interpret this as a real clock pulse and it could cause the bus to hang.

It is recommended that the clock stretching feature is not used.

 

 

Software Development kit.

Example

Version

Issue

Resolution

AFE_Examples SDK 2.3.0.0 The workspace file, AFE_Examples.eww is missing from the AFE_Examples folder. This workspace was intended to allow all of the AFE example projects to be opened in a single workspace. Each of the examples are still present and functional. The workspace file (AFE_Examples.eww) is attached to this document.

Current Profiling

SDK 2.2.0

Lack of Readme

Refer to AN-1282 Application Note in Documentation Folder.

Captouch_5ButtonsTest

SDK 2.2.0

“Right” and “Left” buttons do not work

These pads are used as external interrupts on board. Remove R63 and R65. See Eval-ADuCM350 motherboard schematic for details.

Captouch_5ButtonsTest

SDK 2.2.0

UART Comms Does not work

The simplest fix is to call “test_Init()” after “adi_initpinmux()” instead of before. Baud Rate is 9600.

gpio_test, GpioTest,ThreadSpi.

SDK 2.2.0

Lack of Readme

M5 needs to be connected for VDD_IO supply.

LK14 needs to be inserted for VLCD_VDD supply.

Reveiew Pin-Out for GPIO supplies

Mipi_SSD1963_Test

SDK 2.2.0

No Hardware

This display has been discontinued by supplier. Code is just for reference only.

AmperometricMeasurement SDK 2.2.0 No option to change the value of RCAL or RTIA in software. The functions to set the values of RCAL and RTIA are available in afe.c. See the Amperometric Measurement FAQ for instructions on how to use them and where to insert them. https://ez.analog.com/docs/DOC-11063
Attachments:
ez.analog.com/.../4743.AFE_5F00_Examples.eww.zip
Tags: errata microcontrollers aducm350 sdk known issues aducm35x Precision Microcontrollers Show More
  • Share
  • History
  • More